- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi
I want to translate KBA222517, please confirm to my work.
Regards,
Nino
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi, Nino-san
Confirm to work this KBA.
Thanks
Jenna
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
タイトル:USB 3.0 リンク電力管理状態 - KBA222517
chaitanyav_41が 2018/01/09 23:01 に作成。chaitanyav_41が 2018/01/09 23:02 に変更。
Version: **
質問:
USB 3.0 電源管理状況とは何ですか?
回答:
USB 3.0には、下記で説明される4つのリンク電源状態があります:
U0:フルパワー; データ転送がアクティブ状態
U1:高速リカバリーでのスタンバイ この状態ではデータ転送無しで、電力消費はU0未満
バスアクティビティがない場合、ホスト/デバイスはU1状態へ移行するための要求を出します。他のパートナーは要求を受諾するか拒否できます。他のパートナーが受諾した場合、リンクはU1状態に入ります。それ以外は、U0状態に残ります。その後、リンクパートナーがリンクアクセスの要求をした場合、U1状態を出るためにU1 LFPS出口(LFPSは低周波数定期間信号)コマンドを送ります。最後に、リンクはU0からU1に戻ります。U1からU0への遷移時間はマイクロ秒以内です。
U2:遅い回復でのスタンバイ U2のリンクの電力セーブはU1以上です。
リンクパートナーは下記のように2つの方法でU2に入る事が可能です。
- U0からU2に入る:バスアクティビティがない場合、ホスト/デバイスはU2状態へ移行するための要求を出すことができます。他のパートナーは要求を受諾するか拒否できます。他のパートナーが受諾した場合、リンクはU2状態に移動します。それ以外は、U0状態に残ります。
- U1からU2に入る:
下記2つの条件を満たす場合、U1状態のポートは直接U2に入ります:
1. ポートU2非アクティブタイマーが有効になっている
2. U2非アクティブタイマーがタイムアウトし、U1 LFPS終了信号が受信されない
終了プロセスがU1と同じですが、U2状態から出るためのLFPS終了時間はU1より長くなります。U2からU0への遷移時間はマイクロ秒からミリ秒以内です。
U3:サスペンド状態。 これはもっとも省電力状態のリンクです。ホストのみがデバイスをU3状態に入る事を要求します。デバイスは要求を受諾し、U3状態に入る必要があります。ホストあるいはデバイスのどちらかがU3状態からU0状態に出ることが可能です。U3からU0への遷移時間はミリ秒単位です。
3904 閲覧 カテゴリ: USB: SuperSpeed Peripherals
タグ: bootloader, usb 3.0, fx3, fx3s, fx3 power management, usb 3.0 link power states, u0, u1, u2, u3, low power states in usb 3.0, super-speed low power states