- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I tried to translate following KBA224572 into Japanese.
S6BT112A CXPI Transceiver: Connection with 3.3-V Signals of External IC - KBA224572
===========
Community Translated by
https://community.cypress.com/people/NaTa_2243041
Version **
タイトル:S6BT112A CXPIトランシーバー:外部ICとの 3.3V 信号の接続 - KBA224572
質問:S6BT112A CXPIトランシーバーを外部ICの 3.3V 信号に接続するにはどうすればよいですか?
回答:
(1)入力ピン
CLK(マスターモード時)、TXD、NSLP、およびSELMSの入力電圧特性は次のとおりです。
・ 「H」レベルの入力電圧(min):2 V
・ 「L」レベル入力電圧(max):0.8 V
したがって、LVTTL / LVCMOSとの接続が可能です。
(2)出力ピン
CLK(スレーブモード時)およびRXD端子はオープンドレイン出力です。 抵抗を使用して3.3V にプルアップします。
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello
We receive your translation, it will be published to KBA to Community.
I will get back to you after internal review, after that you will receive the point.
Please bear with me for the delayed the response,
Thanks for your contribution to CDC!
Will keep you update the status.
Thanks,
Jenna Jo