- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I tried to translate following KBA228013 into Japanese.
S6BT112A Behavior when Power Supply Voltage Is Between 4.7 V and 5.3 V – KBA228013
===========
Community Translated by
https://community.cypress.com/people/NaTa_2243041
Version **
タイトル:電源電圧が4.7 V〜5.3 Vの時のS6BT112Aの動作 – KBA228013
S6BT112Aの推奨動作電源電圧の最小値は5.3 Vです。
ローレベルのパワーオンリセットしきい値電圧の最大値は4.7 Vです。
このチップは、電源電圧が4.7 Vから5.3 Vの間で正常に動作するように設計されていますが、
4.7 V〜5.3 Vの電源電圧での電気的特性は、出荷テストでは保証されていません。
----------------------------------------------------------------
Best Regards,
T.Naoki
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello, Naoki-san
We receive your translation, it will be published to KBA to Community.
After upload, You will receive the points as the word of KBA.
Due to the current delay of internal review (Holiday, delayed other works), Please bear with me for the delayed the response.
It could be delayed, but it will be processed soon.
Thanks for your contribution to CDC!
Will keep you update the status.
Thanks,
Jenna Jo