Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Kenshow
Level 8
Level 8
50 solutions authored 25 solutions authored 10 solutions authored

Hi,               

I would like to translate KBA82654 into Japanese.

Please confirm to my work.

Thanks,

Kenshow

2 Replies
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hi, Kenshow-san

Confirm to work this KBA.

Thanks

jenna

Jenna Jo
0 Likes

Hi Jenna-san,

                                

Japanese translation was over.
Please check below.

Original KBA:

Recommended Steps to Dynamically Update the CY22393 PLLs - KBA82654

Thanks.

Kenshow

==============================

タイトル: CY22393 PLLを動的に更新するための推奨手順 - KBA82654

バージョン:**

質問:

PLLを動的に更新する手順は何ですか?

回答:

通常、PLLを動的に更新するには、次の手順をお勧めします。

PLL2またはPLL3の場合:

  1. PLL*_EnビットをLOWに設定して、PLLを無効にします。
  2. PQ、およびPLL*_LF値を再プログラムします。
  3. PLL*_EnビットをHIGHに設定して、PLLを有効にします。

PLL1の場合:
PLL1は、PLL2およびPLL3とは異なります。S2、(S1S0)ピンによって制御される周波数テーブルがあります。SCLK/S1およびSDAT/S0ピンはラッチ入力であり、電源投入時の保持方法に応じて、動作中にアクセス可能なテーブルエントリを決定します。通常、I2Cデータおよびクロックラインにはプルアップがあります。SCLK/S1およびSDAT/S0ピンのプルアップにより、動作中に、ユーザーはS2ピンをトグルして[011]および[111]テーブルエントリにアクセスできます。S2ピンを使用してテーブルエントリ間を切り替える場合、PおよびQ分周器の値ではなく、出力分周器の値のみが変更されると、クロック出力はグリッチなしで新しい周波数を出力します。

たとえば、ユーザーがPLL1テーブルエントリ[011]を使用しているとします。次に、S2HIGHに切り替えると、[111]にアクセスします。

  1. [011]が現在使用されているため、ユーザーはアドレス55H-57H[111]のテーブルエントリ)でPLL値を編集します。
  2. アドレス55H-57Hを設定したら、S2ピンをHIGHに切り替えて、[111]エントリと新しい周波数にアクセスします。
  3. 別の周波数変更が必要な場合は、アドレス49H-4BH[011]のテーブルエントリ)でPLL値を変更します。
  4. アドレス49H-4BHを設定しましたら、S2ピンをLOWに切り替えて、[011]エントリと新しい周波数にアクセスします。

==============================

04-August-2020

  Kenshow

0 Likes