Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
keni_4440091
Level 7
Level 7
500 replies posted 100 solutions authored 50 solutions authored

Dear Supporter

I want to translate the following KBA, please confirm to my work.

Power Sourcing Capabilities of Two Ports in CCG6DF - KBA233121

Regards,

Nino

0 Likes
1 Solution

Dear Jenna

The following shows the translated version in Japanese.

Please confirm and double check.

Regards,

Nino

CCG6DFの2つのポートの電源供給性能 - KBA233121

 

Version: **

 

質問:

 

CCG6DFの両方の内部負荷スイッチは5V/3Aを同時に供給できますか?

 

回答:

 

いいえ。両方のポートは同時に5V/3Aを供給できません。スイッチの一つが5V/3Aを供給している場合、他のポートは最大5V/1.5Aまでしか供給できません。

 

一つのポートが3Aをサポートしている場合、他のポートは最大1.5Aまでサポートできます。測定はパルスモードで行われています。より詳細は、EZ-PD CCG6DF, CCG6SF, USB Type-C Port Controller データシートのDC_NGDO_FET_SYS.2パラメータを参照してください。

 

BGAパッケージのθJAが高いため、接合温度が高すぎると、両方のポートを同時に使用する場合、スイッチの一つの供給電流が1.5Aで限定されます。また、FETはハードウェアの一部として統合されています。

View solution in original post

0 Likes
3 Replies
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hi, Nino-san

Confirm to work this KBA.

Please update the translation in this page.

Thanks,

Jenna 

Jenna Jo
0 Likes

Dear Jenna

The following shows the translated version in Japanese.

Please confirm and double check.

Regards,

Nino

CCG6DFの2つのポートの電源供給性能 - KBA233121

 

Version: **

 

質問:

 

CCG6DFの両方の内部負荷スイッチは5V/3Aを同時に供給できますか?

 

回答:

 

いいえ。両方のポートは同時に5V/3Aを供給できません。スイッチの一つが5V/3Aを供給している場合、他のポートは最大5V/1.5Aまでしか供給できません。

 

一つのポートが3Aをサポートしている場合、他のポートは最大1.5Aまでサポートできます。測定はパルスモードで行われています。より詳細は、EZ-PD CCG6DF, CCG6SF, USB Type-C Port Controller データシートのDC_NGDO_FET_SYS.2パラメータを参照してください。

 

BGAパッケージのθJAが高いため、接合温度が高すぎると、両方のポートを同時に使用する場合、スイッチの一つの供給電流が1.5Aで限定されます。また、FETはハードウェアの一部として統合されています。

0 Likes
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Nino-san,

Thank you for your work for this KBA.

Well received and after released the work, will update to you.

Thank you, 

Jenna Jo
0 Likes