Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Community Translation - PSoC Creator: Invalid Pin Assignment for CapSense External Capacitors – KBA226048

Kenshow
Level 8
Level 8
50 solutions authored 25 solutions authored 10 solutions authored

Hi,

I would like to translate KBA226048 into Japanese.

Thanks,

Kenshow

0 Likes
3 Replies
Kenshow
Level 8
Level 8
50 solutions authored 25 solutions authored 10 solutions authored

Original KBA:

PSoC Creator: Invalid Pin Assignment for CapSense External Capacitors – KBA226048

Translated by Kenshow

==============================

タイトル: PSoC Creator:CapSenseの外付けコンデンサの無効なピン割り当て– KBA226048

バージョン:**

質問:

CmodまたはCshピンがP4 [0]に割り当てられている場合、CapSense®が期待どおりに機能しないのはなぜですか?

回答:

PSoC®4100S Plus、PSoC 4100PS、およびPSoCアナログコプロセッサフ​​ァミリのパーツを使用してデザインを構築する場合、フィッタのルールが正しくないため、CModおよびCshピンをP4 [0]に配置できます。これは、PSoC Creator™バージョン4.2以前に影響します。

回避策:

影響を受けるファミリのパーツを使用する場合、CapSense CmodまたはCshの機能にP4 [0]を使用しないでください。このピンを他の機能として使用できます。

==============================

24-Apr-2020

Kenshow

0 Likes
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello, Kenshow-san,

We receive your translation, it will be published to KBA to Community.

After upload, You will receive the points as the word of KBA.

Due to the current delay of internal review, Please bear with me for the delayed the response.

It could be delayed, but it will be processed soon.

Thanks for your contribution to CDC!

Will keep you update the status.

Thanks,

Jenna Jo

Jenna Jo
0 Likes

Hi,

I reviewed this translation.

The letters in Red is my suggestion for change.

========================

タイトル: PSoC Creator:CapSenseの外付けコンデンサの無効なピン割り当て– KBA226048

バージョン:**

質問:

CmodまたはCshピンがP4 [0]に割り当てられている場合、CapSense®が期待どおりに機能しないのはなぜですか?

回答:

PSoC®4100S Plus、PSoC 4100PS、およびPSoCアナログコプロセッサファミリのパーツを使用してデザインを構築する場合、フィッタのルールに誤りがあるため、CModおよびCshピンをP4 [0]に配置できます。これは、PSoC Creator™バージョン4.2以前に影響します。

回避策:

影響を受けるファミリのパーツを使用する場合、CapSense CmodまたはCshの機能にP4 [0]を使用しないでください。このピン他の機能として使用できます。

========================

13-Oct-2020

Motoo Tanaka

0 Likes