cancel
Showing results for 
Search instead for 
Did you mean: 

Community Translations

keni_4440091
Esteemed Contributor

Dear supporter

I want to translate the following KBA. Please confirm to my work.

PSoC™ 6 MCU with AIROC™ Bluetooth® LE stack events - KBA233928

Regards,

Nino

0 Likes
3 Replies
JennaJo
Moderator
Moderator

Hi, Nino-san

Confirm to work this KBA.

Thanks.

Regards,

Jenna Jo
0 Likes
keni_4440091
Esteemed Contributor

Dear Jenna

The following shows the translated version in Japanese for targeted KBA.

Please conform and double check.

Regards,

Nino

--------------------------------------------------------------------------------------------------

AIROC™ Bluetooth® LEスタックイベント付きPSoC™ 6 MCU – KBA233928

 

Version: **

 

AIROC™ Bluetooth® LE接続付きPSoC™ 6 MCUは、2つのタイプのイベント:Bluetooth® LEスタックイベントおよびサービス固有イベントをサポートします:

 

これらのイベントは、cy_ble_stack.hおよびcy_ble_event_handler.hファイルで定義されます。これらのファイルにアクセスするには、PSoC™ Creatorで、Generated_Source\PSoC6\PDL\Middleware\BLE. In ModusToolbox™ソフトウェアに移動し、libs\blessに移動します。その代わり、https://github.com/Infineon/bless/でこれらのファイルにアクセスできます。

 

Bluetooth® LEスタックイベント: これらのイベントはcy_ble_stack.hで宣言されます。イベントは、enum cy_en_ble_event_tの中で宣言される列挙型データ対応で、以下に示すように分類されます:

 

Generic events: 0x1000 to 0x1FFF
HCI events: 0x2000 to 0x2FFF
Vendor events: 0x3000 to 0x3FFF
GAP events: 0x4000 to 0x4FFF
GATT events: 0x5000 to 0x5FFF
L2CAP events: 0x6000 to 0x6FFF
Qualification events: 0x7000 to 0x7FFF
Future use: 0x8000 to 0xFFFE 

 

サービス固有イベント: これらのイベントはcy_ble_event_handler.hで宣言されます。全てのイベントは、列挙型cy_en_ble_evt_tの中で宣言され、0x10000から開始します。例えば、CY_BLE_EVT_BLSS_INDICATION_ENABLEDは血圧サービスに固有のイベントで、表示が血圧サービス特性を有効にする場合にトリガされます。

 

Labels   MCU & PSoC: PSoC 6

Tags: BHE BLE ble stack gap GATT and L2CAP. hci Add tags

 

JennaJo
Moderator
Moderator

Hi, Nino-san

Thank you for participation on KBA translation.

If there is any issue, I will get back to you.

Thanks. 

Jenna Jo
0 Likes
Top labels