- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I tried to translate this KBA226906 into Japanese.
==========
タイトル:PSoC 4 BLE - 256KB(Bluetooth 4.1)から256KB V2(Bluetooth 4.2)デバイスへの移行
質問:
なぜPSoC 4 BLEの256KB(Bluetooth 4.1)から256KB V2(Bluetooth 4.2)デバイスへの移行が必要ですか?
回答:
2019年1月に、Bluetooth SIGはBluetooth仕様v4.1を正式に廃止しました。Bluetooth仕様v4.1の廃止は新しいBluetoothデザインでは廃止仕様を使用できない事、新しいデザインではアクティブなBluetooth仕様をサポートするシリコンソリューションを使う必要がある事を示しています。そのためサイプレスは、お客様がBluetooth v4.1認定シリコンデバイス(このドキュメントではV1と呼ばれる)からBluetooth v4.2認定シリコンデバイス(V2と呼ばれる)に簡単に移行できるように、このナレッジベースアーティクルを提供しています。サイプレスは、この記事で説明するBluetooth v4.1デバイス毎に互換性のあるドロップインシリコンオプションを提供しています。これらのデバイスのサイプレスの製品終了通知については、PTN191207を参照してください。
質問:どうやってPSoC 4 BLEの256KB(Bluetooth 4.1)から256KB V2(Bluetooth 4.2)デバイスへ移行しますか?
回答:サイプレスは、生産中の全てのBluetooth v4.1デバイスにドロップインコンパチブルなBluetooth v4.2シリコンデバイスを提供しています。
PSoC 4-BLE 256 KB v4.1シリコンデバイスと同等のPSoC 4-BLE 256 KB v4.2デバイスのリストは、表1を参照してください。
ステップに従って、PSoC 4-BLE 256 KB v1デバイスをV2デバイスへ移行します。
ステップ1:V1デバイスを特定する
表1を使用して、「V1」列から使用しているデバイスを見つけ、「V2」列で同等のv4.2デバイスを見つけます。
注意:テープとリールのパッケージオプションは表示されていません。(注文部品番号の末尾に「T」が含まれます)
表1. PSoC 4-BLE 256 KB V1とV2デバイス
デバイス MPN | シリーズ | パッケージ | |
V1 (Bluetooth 4.1) | V2 (Bluetooth 4.2) | ||
CY8C4128FNI-BL443 | CY8C4128FNI-BL543 | PSoC 4100 BLE | 76-WLCSP |
CY8C4128FNI-BL453 | CY8C4128FNI-BL553 | PSoC 4100 BLE | 76-WLCSP |
CY8C4128FNI-BL463 | CY8C4128FNI-BL563 | PSoC 4100 BLE | 76-WLCSP |
CY8C4128FNI-BL473 | CY8C4128FNI-BL573 | PSoC 4100 BLE | 76-WLCSP |
CY8C4128FNI-BL483 | CY8C4128FNI-BL583 | PSoC 4100 BLE | 76-WLCSP |
CY8C4128FNI-BL493 | CY8C4128FNI-BL593 | PSoC 4100 BLE | 76-WLCSP |
CY8C4128LQI-BL443 | CY8C4128LQI-BL543 | PSoC 4100 BLE | 56-QFN |
CY8C4128LQI-BL453 | CY8C4128LQI-BL553 | PSoC 4100 BLE | 56-QFN |
CY8C4128LQI-BL463 | CY8C4128LQI-BL563 | PSoC 4100 BLE | 56-QFN |
CY8C4128LQI-BL473 | CY8C4128LQI-BL573 | PSoC 4100 BLE | 56-QFN |
CY8C4128LQI-BL483 | CY8C4128LQI-BL583 | PSoC 4100 BLE | 56-QFN |
CY8C4128LQI-BL493 | CY8C4128LQI-BL593 | PSoC 4100 BLE | 56-QFN |
CY8C4248FNI-BL443 | CY8C4248FNI-BL543 | PSoC 4200 BLE | 76-WLCSP |
CY8C4248FNI-BL453 | CY8C4248FNI-BL553 | PSoC 4200 BLE | 76-WLCSP |
CY8C4248FNI-BL463 | CY8C4248FNI-BL563 | PSoC 4200 BLE | 76-WLCSP |
CY8C4248FNI-BL473 | CY8C4248FNI-BL573 | PSoC 4200 BLE | 76-WLCSP |
CY8C4248FNI-BL483 | CY8C4248FNI-BL583 | PSoC 4200 BLE | 76-WLCSP |
CY8C4248FNI-BL493 | CY8C4248FNI-BL593 | PSoC 4200 BLE | 76-WLCSP |
CY8C4248FNQ-BL483 | CY8C4248FNQ-BL583 | PSoC 4200 BLE | 56-QFN |
CY8C4248LQI-BL443 | CY8C4248LQI-BL543 | PSoC 4200 BLE | 56-QFN |
CY8C4248LQI-BL453 | CY8C4248LQI-BL553 | PSoC 4200 BLE | 56-QFN |
CY8C4248LQI-BL463 | CY8C4248LQI-BL563 | PSoC 4200 BLE | 56-QFN |
CY8C4248LQI-BL473 | CY8C4248LQI-BL573 | PSoC 4200 BLE | 56-QFN |
CY8C4248LQI-BL483 | CY8C4248LQI-BL583 | PSoC 4200 BLE | 56-QFN |
CY8C4248LQI-BL493 | CY8C4248LQI-BL593 | PSoC 4200 BLE | 56-QFN |
CY8C4248LQQ-BL483 | CY8C4248LQQ-BL583 | PSoC 4200 BLE | 56-QFN |
CY8C4248FLI-BL483 | CY8C4248FLI-BL583 | PSoC 4200 BLE | 76-WLCSP (thin) |
CYBLE-212019-00 | CYBLE-212020-01 | PSoC 4200 BLE Module | 31-SMT |
CYBLE-214009-00 | CYBLE-214015-01 | PSoC 4200 BLE Module | 32-SMT |
CYBLE-222005-00 | CYBLE-222014-01 | PSoC 4200 BLE Module | 22-SMT |
CYBLE-224110-00 | CYBLE-224116-01 | PSoC 4200 BLE Module | 32-SMT |
PSoC Creator™プロジェクトがある場合、次の手順を使用して、V1デバイスを使用するかどうか判断できます。
- PSoC Creatorの最新バージョンでプロジェクトを開きます。推奨する最小バージョンはPSoC Creator4.2です。
デバイスによっては、PSoC Creatorが廃止デバイスリストのポップアップウィンドウを表示する場合があります。現在のデバイスとして指定されているデバイスが表1の「V1」列に列挙されている場合、廃止されたV1デバイスを使っています。ステップ2へ進み、適切なV2デバイスを特定します。図1.Obsolete Device ポップアップ表示 - 「Obsotete Device」ダイアログが表示されなかった場合、PSoC Creator IDEウィンドウでプロジェクトが開きます。図2に示すように、Workspace Explorerパネルでプロジェクト名と一緒に表示されているデバイスの部品番号を見つけます。このデバイスが表1の「V1」列に列挙されている場合、V1デバイスを使っています。ステップ2へ進み、適切なV2デバイスを特定します。
図2. Workspace Explorerのデバイス名
ステップ2. 適切なV2デバイスを特定する
表1の「V2」列は、V1デバイスと対応するパッケージとピン互換のV2デバイスを列挙しています。
表1に示す「V2」デバイスは、同等の「V1」デバイスのフォームフィットファンクション互換のシリコンデバイスです。正確なフォームフィットファンクションの「V2」を置き換えるには、表1の「V2」デバイスをメモしてステップ3へ進みます。
フットプリントが互換性のあるソリューションのみ必要で、機能差に問題がない場合は、同じパッケージタイプが列挙されている任意のデバイスから選択できます。図5に示すようにフィルターのBluetooth = 4.2に設定して、PSoC Creator内のDevice Selectorを使用する事も出来ます。この画面では、全てのV2デバイスを表示し、列を使用して機能を比較して、要件に一致するデバイスを特定できます。フットプリントの互換性のために、「Package」列は現在の「V1」デバイスと一致するパッケージでフィルターする必要がある事に注意してください。
ステップ3. PSoC Creatorプロジェクトを更新する
このステップは、V1デバイス用のPSoC Creatorプロジェクトがあり、V2デバイスを使用するよう更新する場合に適用します。
- PSoC Creatorの最新バージョンで現在のプロジェクトを開きます。推奨する最小バージョンはPSoC Creator4.2です。
- 図3に示すように「Obsolete Device」ポップアップが表示された場合は、(choose another replacement) をクリックします。これにより、Device Selectorウィンドウが開きます。ステップ4へ進みます。
図3. Obsolete Device ウィンドウ - 「Obsolete Device」ウィンドウが表示されなかった場合、プロジェクトは引き続きPSoC Creator IDEで開きます。図4に示すように、Workspace Explorerでプロジェクト名を右クリックし、Device Selectorを選択します。
図4. Device Selectorを開く - 図5で示すようにフィルターを変更してV2デバイスを選択します。
- Flash (KB) = 256と、Bluetooth = 4.2 でフィルターを使用します。これによりリストが絞り込まれ、PSoC 4 BLE 256 KB V2 (Bluetooth 4.2デバイス)のみが表示されます。
- ステップ2で特定したV2デバイスをリストから選択します。
- OKをクリックして選択を適用します。
図5. V2デバイスを表示するDevice Selectorフィルター
- BLEコンポーネントを最新バージョンに更新します。
- プロジェクト名を右クリックして、Update Componentsを選択します。
図6. Update components - BLEコンポーネントのNew Versionドロップダウンリストを使用して、利用可能な最新のBLEコンポーネントバージョンを選択し、Nextをクリックします。
図7. BLEコンポーネントを利用可能な最新バージョンへ更新 - 必要に応じて、Create workspace archive before updating オプションを選択して現在のプロジェクトのバックアップアーカイブを作成します。Finishをクリックしてコンポーネントの更新をプロジェクトに適用します。
図8. コンポーネント更新完了
- プロジェクト名を右クリックして、Update Componentsを選択します。
- Build > Clean and Build <project name> を使用して、プロジェクトをビルドします。Output Consoleでビルドが成功したことを確認します。
これでプロジェクトがV2デバイスに正常に移行されました。
==========
BR,
Omoi
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello, Omoi-san
We receive your translation, it will be published to KBA to Community.
It will be reviewed internally.
After upload, You will receive the points as the word of KBA.
Due to the current volume of works (waiting review, etc.), Please bear with me for the delayed the response.
It could be delayed, but it will be processed soon.
Thanks for your contribution to CDC!
Will keep you update the status.
Thanks,
Jenna Jo
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello, Omoi-san
Thanks for waiting for long time,
Your translation has been published to Community.
You will receive the point as a token of appreciation.
Thanks for your contribution.
Regards,
Jenna