Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Kenshow
Level 8
Level 8
50 solutions authored 25 solutions authored 10 solutions authored

Hi,               

I would like to translate KBA203597 into Japanese.

Please confirm to my work.

Thanks,

Kenshow

2 Replies
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hi, Kenshow-san

Confirm to work this KBA.

Thanks,

Jenna

Jenna Jo
0 Likes

Hi Jenna-san,

                                

Japanese translation was over.
Please check below.

Original KBA:

Migrating from SST25VF064C to S25FL064P, does the 4KB sub-sector erase work in the same manner? - KB...

Thanks.

Kenshow

==============================

タイトル: SST25VF064CからS25FL064Pに移行すると、4KBサブセクターの消去は同じように機能しますでしょうか?- KBA203597

バージョン:**

質問:

SST25VF064CからS25FL064Pに移行すると、4KBサブセクターの消去は同じように機能しますでしょうか?

回答:

S25FL064P SPI FLASHデバイスは、128 KBの均一な64 kBセクターで構成され、2つ(上部または下部)の64 kBセクターがさらに32個の4 kBサブセクターに分割されます。メインメモリアレイ内の残りのセクターは専用の64KBセクターで、4KBサブセクターを含まず、4KBP4E)サブセクター消去コマンド20hをサポートしていません。これらの専用の64 KBセクターを部分的に(4 KB)消去することはできません。したがって、消去される実際のセクターに応じて、4 KBのサブセクター消去がサポートされるかどうかが決まります。

2つの上部または下部の64 KBセクターのみに4KBサブセクターがあり、4 KBP4E)サブセクター消去コマンド20hをサポートしています。SST25VF064C SuperFlashメインメモリアレイは、メインメモリアレイ全体で、32 KBのオーバーレイブロックと64 KBのオーバーレイの消去可能なブロックを備えた、4 KBの均一な消去可能なセクターで構成されています。

==============================

14-Sept-2020

Kenshow

0 Likes