Community Translation - Migrating from 48-FBGA MRAM to 60-FBGA nvSRAM - KBA218078

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
MiNe_85951
Level 7
Level 7
Distributor - TED (Japan)
50 likes received 500 replies posted 50 solutions authored

Dear Sirs and  Madams,

I would like to translate KBA218078, please confirm to my work

Regards,

Masashi

0 Likes
2 Replies
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Masashi-san

Yes, confirm of it.

It is good to work.

Thanks,

Jenna

Jenna Jo
0 Likes
MiNe_85951
Level 7
Level 7
Distributor - TED (Japan)
50 likes received 500 replies posted 50 solutions authored

Jenna-san,

I translated KBA218078 into Japanese.

We would appreciate it if you could confirm.

Regards,

Masashi

/***************************************************************************************/

Migrating from 48-FBGA MRAM to 60-FBGA nvSRAM - KBA218078

48-FBGA MRAMから60-FBGA nvSRAMへの移行 - KBA218078

Version: **

質問:

48-FBGA MRAMから60-FBGA nvSRAMへデバイスを移行するときに必要な手順は何ですか?

回答:

サイプレスは16Mb nvSRAMを60ボールFBGAパッケージで提供しています。

MRAM(48ボールFBGA)からnvSRAMに移行する場合、フットプリントに基づいた以下の変更を行う必要があります。


1. nvSRAMパッケージのコーナーに12個で構成されたVssパッド作成します。
2. MRAMのボールA6(NC)をnvSRAMのボールC8(CE2)であるVccに接続します。
3. MRAMのボールE3(DC)をフローティングにするか、nvSRAMのボールG5(HSB#)であるVccにプルアップします。

 Vssにショートしないでください。
4. nvSRAMパッケージのボールJ4(Vcap)に相当する、MRAMボールG2にコンデンサ(標準 22 µF +/- 10%、絶対範囲 19.8 µF〜82 µF)を追加します。

1.png

パッケージ外形寸法

2.png

0 Likes