Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Community Translation - Meaning of AEC-Q100 – KBA220733

Kenshow
Level 8
Level 8
50 solutions authored 25 solutions authored 10 solutions authored

Hi,               

I would like to translate KBA220733 into Japanese.

Please confirm to my work.

Thanks,

Kenshow

0 Likes
2 Replies
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hi, Kenshow-san

Confirm to work this KBA.

Thanks,

Jenna

Jenna Jo
0 Likes

Hi Jenna-san,

                                

Japanese translation was over.
Please check below.

Original KBA:

Meaning of AEC-Q100 – KBA220733

Thanks.

Kenshow

==============================

タイトル: AEC-Q100の意味 – KBA220733

バージョン:*A

質問: AEC-Q100の定義と目的は何でしょうか?

回答:

AEC-Q100は、 Automotive Electronics CouncilAEC)によって開発された、集積回路の一連の認定試験シーケンスです。AEC-Q100は、自動車電子機器の一般的な部品認定および品質システム規格を確立し、自動車アプリケーションに組み込まれたパッケージ化された集積回路の推奨される新製品および主要な変更認定の要件と手順の概要を示す業界標準仕様です。

http://www.aecouncil.com/AECDocuments.htmlAEC-Q100仕様をご参照願います。

自動車用途に適格な製品は、AEC-Q100要件を満たし、表1で次の自動車用温度グレードのラベルが付いている場合があります。

1.自動車用温度グレード

グレード

使用周囲温度範囲

0

-40°Cから+ 150°C

1

-40°Cから+ 125°C

2

-40°Cから+ 105°C

3

-40°Cから+ 85°C

注:サイプレスは現在、AEC-Q100の注文オプションとしてGrade-1Grade-2Grade-3を提供しています。

==============================

8-July-2020

Kenshow

0 Likes