Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Community Translation - Maximum Current in HX2VL Bus-Powered Configuration – KBA228350

Kenshow
Level 8
Level 8
50 solutions authored 25 solutions authored 10 solutions authored

Hi,

I would like to translate KBA228350 into Japanese.

Please confirm to my work.

Thanks,

Kenshow

0 Likes
2 Replies
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello, Kenshow-san

Confirm to work this KBA.

Thanks

Jenna

Jenna Jo
0 Likes

Hi Jenna-san,

                                

Japanese translation was over.
Please check below.

Original KBA:

Maximum Current in HX2VL Bus-Powered Configuration – KBA228350

Thanks.

Kenshow

==============================

タイトル: HX2VLバスパワー構成の最大電流 – KBA228350

バージョン:**

質問:バスパワーHX2VLに接続されている場合、デバイス構成の電流制限を100 mAより大きくできますか?

回答:いいえ。バスパワー2.0ハブに接続されたデバイスの電流制限は100 mAを超えることはできません。これは、バスパワーの場合、HX2VLデバイスを使用してハイパワーデバイスに電力を供給することができないことを意味します。

ホストは、バス駆動のアップストリームポートに500 mAを割り当てます。4ポートHX2VLハブが接続されている場合、ハブは内部使用で約100 mAを消費します。これにより、各ポートで最大100 mAが残ります。

ただし、2つのダウンストリームポートに接続されている2つのデバイスがあり、他の2つが無効になっているポートであっても、デバイスは、たとえば、それぞれ200 mAを引き込むことができません。

詳細については、Guidelines on System Design Using Cypress’ USB 2.0 Hub (HX2VL)サイプレスのUSB 2.0ハブ(HX2VL)を使用したシステム設計のガイドラインを参照してください。

==============================

2-June-2020

Kenshow

0 Likes