Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

KaKi_1384211
Level 6
Level 6
100 replies posted 50 replies posted 50 questions asked

【タイトル】

128Mbit以上の大容量SPI Flash Memory(S25FL-Sシリーズ) へアクセスする従来の3Byteアドレスによるアドレッシング方法 - KBA203748

【質問】

従来の3Byteアドレスによりアドレッシング方法を使用して、128Mbit以上のSPI Flash Memoryへアクセスするためのオプションはありますか?

【回答】

はい、Cypress S25FL-Sシリーズには、従来の3Byteアドレスを使用して、128Mbit以上のSPI Flash Memoryへアクセスするためのオプションがあります。

Cypress “Bank Address Register”(BAR) を使用することにより、この3Byteアドレスによるアドレッシング方法を提供しています。

128Mbit以上へアクセスするための3Byteアドレスによるアドレッシング方法は、Bank Address Register(BAR) bit7(EXTADO) “0”(デフォルト) で保持します。

その上で、Bank Address Register(BAR) bit0(BA24)、及び bit1(BA25) “0”、及び “1” にすることにより、128Mbit以上のアドレスを設定します。

このBank Address Register(BAR) 2bit(bit0bit1) の組み合わせにより、3Byteアドレスコマンド、かつ 3Byteアドレッシングを使用して、

最大512MbitMemoryエリアへアクセスすることができます。

詳細については、該当製品のデータシートを確認してください。

また、Bank Address Register(BAR)に対応する製品はCypress S25FL-Sシリーズのみです。

1 Reply
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello,

We receive your translation, it will be published to KBA to Community.

After upload, You will receive the points as the word of KBA.

Due to the current delay of processed work, Please bear with me for the delayed the response.

It could be delayed, but it will be processed soon.

Thanks for your contribution to CDC!

Will keep you update the status.

Thanks,

Jenna Jo

Jenna Jo
0 Likes