Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
KoKi_1693136
Level 5
Level 5
Distributor - Marubun (Japan)
5 solutions authored 25 replies posted First solution authored

Hi,

I tried to translate following one into Japanese.

Land Pattern Recommendations for Commonly Used Cypress Packages – KBA225416

https://community.cypress.com/docs/DOC-16633

=========================

質問:

良く使用されている Cypress パッケージ用の推奨ランドパターンはどのようなものがありますか?

回答:

良く使用されている Cypress のパッケージには以下のようなものがあります。

100-Ball Ball Grid Array (6.0 × 6.0 × 1.0 mm)

100 Ball BGA

44-Pin Thin Small Outline Package Type II

44 Pin TSOP II

54-Pin Thin Small Outline Package Type II

54 Pin TSOP II

48-Pin Thin Small Outline Package Type I

48 Pin TSOP I

28-Pin Thin Small Outline Package

28 Pin TSOP

64-Ball Fortified Ball Grid Array (13 x 11 mm)

64 Ball FBGA 13x11

8-Pin Small Outline Integrated Circuit (208 mils)

8 Pin SOIC 208 mils

8-Pin Dual Flat No Leads (5x6x0.75 mm)

8 Pin DFN

8-Pin Ultra-Thin Small Outline No-lead Package

8 Pin USON

64-Ball Fortified Ball Grid Array (9x9mm)

64 Ball FBGA 9x9

16-Pin Quad Flat No-Leads (3 x 3 x 0.6 mm)

16 Pin QFN

8-Pin Small Outline Integrated Circuit (150 mils)

8 Pin SOIC 150 mils

100-Pin Thin Quad Flat Package (14 x 14 x 1.4 mm)

6-pin Ceramic LCC (5 x 3.2 x 1.30 mm)

8-pin Quad Flat No-Leads (3.28 x 3.28 x 0.55 mm)

16-pin Small Outline Integrated Circuit

24-pin Quad Flat No-Leads

32-Pin Thin Small Outline Package Type II

32-Pin Thin Small Outline Package Type I

48-pin Quad Flat No-Leads

48-Ball Very Fine Pitch Ball Grid Array

361-Ball Flip Chip Ball Grid Array

100 Pin TQFP

6 pin LCC

8 pin GQFN

16 pin SOIC

24 pin QFN

32 pin TSOP II

32 pin TSOP I

48 pin QFN

48 Ball VFBGA

361 Ball FCBGA

1 Reply
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello,

We receive your translation, it will be published to KBA to Community.

After upload, You will receive the points as the word of KBA.

Due to the current volume of works, Please bear with me for the delayed the response,

Thanks for your contribution to CDC!

Will keep you update the status.

Thanks,

Jenna Jo

Jenna Jo