Community Translation - Increasing S6BP202A Rated Output Current under Low Input Voltage Condition – KBA226161

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Kenshow
Level 8
Level 8
Distributor - Marubun (Japan)
50 solutions authored 25 solutions authored 10 solutions authored

Hi,               

I would like to translate KBA226161 into Japanese.

Please confirm to my work.

Thanks,

Kenshow

0 Likes
2 Replies
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hi, Kenshow-san

Confirm to work this KBA.

Thanks

Jenna

Jenna Jo
0 Likes
Kenshow
Level 8
Level 8
Distributor - Marubun (Japan)
50 solutions authored 25 solutions authored 10 solutions authored

Hi Jenna-san,

                                

Japanese translation was over.
Please check below.

Original KBA:

Increasing S6BP202A Rated Output Current under Low Input Voltage Condition – KBA226161

Thanks.

Kenshow

==============================

タイトル: 低入力電圧条件下でのS6BP202A定格出力電流の増加 – KBA226161

バージョン:**

質問:

低入力電圧条件下でS6BP202Aの定格出力電流をどのように増加させることができますか?

回答:

スイッチング周波数を下げて、低入力電圧でのS6BP202Aの定格出力電流を増やします。

1は、デフォルトのスイッチング周波数2.1 MHzでのIVOUT vs VVINのグラフを示しています。例えば、VVIN = 3.5VTa = + 25°C)の場合、定格出力電流は約0.7 A です。

 

1.  IVOUT vs VVINのグラフ

pastedImage_4.png  

スイッチング周波数を200 kHzに設定すると、図2に示すように、VVIN = 3.5VTa = + 25°C)のときに定格出力電流が1.2 Aに増加します。

2. IVOUT vs VVINのグラフ

pastedImage_15.png  

スイッチング周波数を200 kHzに設定するには、次のコンポーネント値を使用します。

設定抵抗(RT= 270kΩ

インダクタ(L= 22μHCLF12577NIT-220M-D

入力コンデンサ(CIN= 10μF

出力コンデンサ(COUT)のオプションのいずれかを選択します。

オプション1

項目

セラミックCGA6P1X7R1C226M250AC

8

オプション2

項目

高分子電解HHXD160ARA151MF80G

1

セラミックCGA6P1X7R1C226M250AC

1

スイッチング周波数の設定方法の詳細についてはAN99497セクション2.1.3S6BP201AS6BP202A、およびS6BP203A使用した電源管理システムの設計」を参照してください。

==============================

23-June-2020

Kenshow

0 Likes