Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

keni_4440091
Level 7
Level 7
500 replies posted 100 solutions authored 50 solutions authored

Hi

Please let me translate this topic in Japanese language.

Regards,

Nino

2 Replies
keni_4440091
Level 7
Level 7
500 replies posted 100 solutions authored 50 solutions authored

Increase BLE Data Rate - KBA224929

タイトル:BLEデータレートの増加 - KBA224929

バージョン 4

chaitanyav_412018/08/31 2:46 に作成。ChaitanyaV_612019/08/12 21:00 に変更。

Author: ShengY_96      Version: **

質問:

2つのBLEデバイス間でどのようにしてブルートゥースローエナジー(BLE)データレートを増やしますか?

回答:

一般的に、BLEデータレートはATT_MTU、コネクションインターバル、リンクレイヤペイロード(BLE4.2: LLペイロード=251)、BLE物理データレート(BLE5.02Mbpsをサポート)に関連しています。BLEデータレートを増やすためには、4つのパラメータで調整して下さい。

BLE 5.0ではBLE 4.2 1Mbpsに比べると2M PHYがサポートされます。BLE 5.0で実現される理論的アプリケーションデータレートはおよそ1.4 Mbpsになります。

BLE 4.2ではリンクレイヤペイロードはBLE 4.127バイトに比べると251バイトまであります。BLE 4.2で実現される理論的アプリケーションデータレートはおよそ800 kbpsになります。

BLE 4.1での理論的アプリケーションデータレートはおよそ300 kbpsになります。

BLEコミュニケーションではクライアントやサーバーの両方の協力が必要です。BLEデバイスが電話に接続されている場合、電話の接続間隔、ATT_MTUサイズおよび電話のOS制限により実データレートは理想値よりも低くなります。データレートを増価するためには、最初にサーバーおよびクライアント側でATT_MTUの値(23から512まで)を大きく、例えば512に設定にしてください。次に、接続間隔を適切に設定してください。一般的に最小接続間隔では電話接続のデータレートが高くなる場合があります。最後に、クライアントとサーバーの両方がBLE 4.2LE 2M PHYをサポートしている場合は、リンクレイヤペイロードを251バイトに設定し、2M PHYを使用して下さい。

本説明はリンクレイヤデータ詳細に役立つ場合があります。

376 閲覧 カテゴリ: Other タグ: wireless, ble, data rate, psoc ble, wiced ble

0 Likes
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello, Nino-san

We receive your translation, it will be published to KBA to Community.

After upload, You will receive the points as the word of KBA.

Due to the current delay of processed work, Please bear with me for the delayed the response.

It could be delayed, but it will be processed soon.

Thanks for your contribution to CDC!

Will keep you update the status.

Thanks,

Jenna Jo

Jenna Jo
0 Likes