Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

taas_3144281
Level 5
Level 5
25 sign-ins 50 replies posted 25 replies posted

Hi,

I tried to translate this KBA226843 into Japanese.

IMO Accuracy for PSoC 4 - KBA226843

--------------------------------------------

タイトル

PSoC 4のIMO精度について - KBA226843

質問:

PSoC®4のIMO周波数精度はどのくらいですか、それはなぜ制限されているのですか?

回答:

内部主発振器の精度は±2%です。PSoCデバイスでは、WCO(32 kHz時計用水晶発振器)を使用して、IMOの精度を動的に±0.2%へ調整できます。IMOブロックはハードウェア制御の周波数トリムレジスタを2つ提供します。CLOCK_TRIM_1レジスタはIMO出力を120 kHzステップで制御し、CLOCK_TRIM_2レジスタは15 kHzステップでより細かい制御をします。その結果、IMOの精度は±15 kHzとなります。±15kHzの精度は、8 MHz IMOで約±0.2%に変換され、クロックの精度をより高いものにします。

--------------------------------------------

Best Regards,

Asanuma

0 Replies