Apr 06, 2020
01:00 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Apr 06, 2020
01:00 AM
Hi,
I tried to translate this KBA226843 into Japanese.
IMO Accuracy for PSoC 4 - KBA226843
--------------------------------------------
タイトル
PSoC 4のIMO精度について - KBA226843
質問:
PSoC®4のIMO周波数精度はどのくらいですか、それはなぜ制限されているのですか?
回答:
内部主発振器の精度は±2%です。PSoCデバイスでは、WCO(32 kHz時計用水晶発振器)を使用して、IMOの精度を動的に±0.2%へ調整できます。IMOブロックはハードウェア制御の周波数トリムレジスタを2つ提供します。CLOCK_TRIM_1レジスタはIMO出力を120 kHzステップで制御し、CLOCK_TRIM_2レジスタは15 kHzステップでより細かい制御をします。その結果、IMOの精度は±15 kHzとなります。±15kHzの精度は、8 MHz IMOで約±0.2%に変換され、クロックの精度をより高いものにします。
--------------------------------------------
Best Regards,
Asanuma
0 Replies