Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Community Translation - How to Change the UART Baud Rate During the Runtime on PSoC - KBA230021

Kenshow
Level 8
Level 8
50 solutions authored 25 solutions authored 10 solutions authored

Hi,

I would like to translate KBA230021 into Japanese.

Thanks,

Kenshow

0 Likes
2 Replies
Kenshow
Level 8
Level 8
50 solutions authored 25 solutions authored 10 solutions authored

Original KBA: KBA230021

How to Change the UART Baud Rate During the Runtime on PSoC - KBA230021

Translated by Kenshow

==============================

タイトル: PSoCの動作中にUARTボーレートを変更する方法 - KBA230021

バージョン:**

1. 1示すように、コンポーネントカタログからUARTコンポーネントを選択し、* TOPDesign.cyschタブに配置します。

1. UARTコンポーネントをTOPDesign.cyschに配置する

KBA230021_1.png

2. 図2が示すように、UARTコンポーネントをダブルクリックし、Configure ‘UART’ Clock Terminaを有効にします

図2. UARTコンポーネントの構成

KBA230021_2.png

3.   図3示すように、最初に必要なボーレートに従って、外部クロックをUARTコンポーネントに接続し、クロックの周波数を設定ます

図3. UARTコンポーネントへの外部クロックの追加

KBA230021_3.png

4. 実行時に、次のコードスニペットに示すように、Clock_SetDivider(uint16 Divider)を使用してUARTのボーレートを変更することにより、クロックディバイダーの値を変更してボーレートを変更します(ボーレートは9600に設定されています。ボーレートは クロック設定の分周値に応じて、および適切な外部クロック周波数を設定することによって変更されます)

KBA230021_3_5.png

5. 今、実際のボーレートは9607 bpsに設定されています。

図4.ボーレートの設定

KBA230021_4.png

==============================

15-Apr-2020

Kenshow

JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello, Kenshow-san

We receive your translation, it will be published to KBA to Community.

It will be reviewed internally.

After upload, You will receive the points as the word of KBA.

Due to the current volume of works (waiting review, etc.), Please bear with me for the delayed the response.

It could be delayed, but it will be processed soon.

Thanks for your contribution to CDC!

Will keep you update the status.

Thanks,

Jenna Jo

Jenna Jo