Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Community Translation - FX3 UART Prints Garbage Data During JTAG Debugging - KBA86728

Kenshow
Level 8
Level 8
50 solutions authored 25 solutions authored 10 solutions authored

Hi,

I would like to translate KBA86728 into Japanese.

Please confirm to my work.

Thanks,

Kenshow

0 Likes
2 Replies
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello, Kenshow-san

Yes, Confirm the KBA.

Please work to do.

Thanks,

Jenna

Jenna Jo
0 Likes

Hi Jenna-san,

Japanese translation was over.
Please check below.

Original KBA:

FX3 UART Prints Garbage Data During JTAG Debugging - KBA86728

Thanks.

Kenshow

==============================

タイトル: FX3 UARTがJTAGデバッグ中に不要なデータを出力する - KBA86728

バージョン:*A

質問:EzUsbSuite_UG.pdfの第3章で説明されているように)JTAGインターフェイスを介してFX3ファームウェアをデバッグすると、UARTは不要なデータを送信します。ただし、ボードでの通常のファームウェア実行中は正しく動作します(JTAGデバッグなし)。なぜでしょうか?

回答:

これは、Eclipseでデバッグ環境をセットアップするときに渡された誤った初期化コマンドが原因であると考えられます。UARTを介した不要なデータの送信を回避するには、JTAG初期化中にFX3 CPUクロックを正しく設定する必要があります。

1示すように、必要な入力クロック設定に対応するコマンドをDebug Configuration設定の[ Startup ]タブに追加します

  • 19.2 MHzの場合、monitor memU32 0xE0052000 = 0x00080015
  • 26.0 MHzの場合、monitor memU32 0xE0052000 = 0x00080010
  • 38.4 MHzの場合、monitor memU32 0xE0052000 = 0x00080115
  • 52.0 MHzの場合、monitor memU32 0xE0052000 = 0x00080110

1. Debug Configuration設定の[ Startup ]タブ

1.png  

コマンド「monitor sleep 1000」は、クロックを安定させるために使用されます。

==============================

19-May-2020

Kenshow

0 Likes