Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
keni_4440091
Level 7
Level 7
500 replies posted 100 solutions authored 50 solutions authored

Dear supporter

I want to translate the following KBA. Please confirm to my work.

FX3: Questions on Self-Powered Design – KBA233244

Regards,

Nino

0 Likes
1 Solution

Dear Jenna

The following shows the translation in Japanese for targeted KBA.

Please confirm and double check.

Regards,

Nino

---------------------------------------------------------------------

FX3: セルフ-パワー設計に関する質問 – KBA233244

 

Version: **

 

質問1 FX3がセルフ‐パワーデバイスとして使用されている場合、どのようにUSB I/Oへ電源供給しますか?

 

回答: USB I/Oは、3.3-Vの安定化電源を必要とします。この電源は、外部電源のVBUSか、またはVBATTのどちらかから内部駆動されます。USBポートが使用されている場合、1つまたは両方の電源が必要になります。FX3セルフ-パワー設計では、VBATTはシステムバッテリ、またはPMICからの安定化3.2V-6V電圧レールに接続できます。FX3のVBUSピンはアップストリームUSB接続を検出するためにUSBコネクタのVBUSに接続できます。VBUSとVBATTの両方があり、指定された範囲にある場合、VBUSはUSB I/Oに対して主要電源になります。FX3デバイスは、ソフトウェア/ファームウェアオーバーライドがなければ、デフォルトでVBUS電源から電力を引きます。FX3のUSBブロックは、CyU3PUsbVBattEnable APIを使用したVBUSの代わりにVBATT電源で動作する構成にできます。APIに関する詳細は、FX3 SDKからFX3 APIガイドを参照してください。

 

質問2 FX3 VBUSピンがUSBコネクタのVBUS信号に接続されてない場合、どのファームウェア変更が必要ですか?

 

回答: FX3がUSBデバイスとして機能している場合、デフォルトでVBUS検出を実行し、VBUS電圧が4.1Vを超えている時のみホストに接続します。FX3のVBUSが未接続のままの状態の場合、ユーザーは、適切な時間にファームウェアのUSB接続を有効化/無効化にする必要があります。この場合、CyU3PUsbControlVBusDetect APIの有効およびuseVbattパラメータの両方は、CyFalseに設定される必要があり、CyU3PConnectState APIはユーザーアプリケーションによって直接呼び出される必要があります。質問1で述べたように、CyU3PUsbVBattEnable APIを使用して、代わりにVBATTから電力をデバイスに供給します。

 

注意: FX3 PMODEラインがUSB ブート(Z11)として構成され、VBUSピンがUSBコネクタのVBUS信号に接続されていない場合、デバイスは列挙されません。この場合、USBブート以外のブートオプション用にPMODEラインを構成することを推奨します。

 

Labels  Other

Tags: fx3 self-powered vbatt vbus Add tags

View solution in original post

0 Likes
3 Replies
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hi, Nino-san

Confirm to work this KBA.

Thanks,

Best regards, 

Jenna Jo
0 Likes

Dear Jenna

The following shows the translation in Japanese for targeted KBA.

Please confirm and double check.

Regards,

Nino

---------------------------------------------------------------------

FX3: セルフ-パワー設計に関する質問 – KBA233244

 

Version: **

 

質問1 FX3がセルフ‐パワーデバイスとして使用されている場合、どのようにUSB I/Oへ電源供給しますか?

 

回答: USB I/Oは、3.3-Vの安定化電源を必要とします。この電源は、外部電源のVBUSか、またはVBATTのどちらかから内部駆動されます。USBポートが使用されている場合、1つまたは両方の電源が必要になります。FX3セルフ-パワー設計では、VBATTはシステムバッテリ、またはPMICからの安定化3.2V-6V電圧レールに接続できます。FX3のVBUSピンはアップストリームUSB接続を検出するためにUSBコネクタのVBUSに接続できます。VBUSとVBATTの両方があり、指定された範囲にある場合、VBUSはUSB I/Oに対して主要電源になります。FX3デバイスは、ソフトウェア/ファームウェアオーバーライドがなければ、デフォルトでVBUS電源から電力を引きます。FX3のUSBブロックは、CyU3PUsbVBattEnable APIを使用したVBUSの代わりにVBATT電源で動作する構成にできます。APIに関する詳細は、FX3 SDKからFX3 APIガイドを参照してください。

 

質問2 FX3 VBUSピンがUSBコネクタのVBUS信号に接続されてない場合、どのファームウェア変更が必要ですか?

 

回答: FX3がUSBデバイスとして機能している場合、デフォルトでVBUS検出を実行し、VBUS電圧が4.1Vを超えている時のみホストに接続します。FX3のVBUSが未接続のままの状態の場合、ユーザーは、適切な時間にファームウェアのUSB接続を有効化/無効化にする必要があります。この場合、CyU3PUsbControlVBusDetect APIの有効およびuseVbattパラメータの両方は、CyFalseに設定される必要があり、CyU3PConnectState APIはユーザーアプリケーションによって直接呼び出される必要があります。質問1で述べたように、CyU3PUsbVBattEnable APIを使用して、代わりにVBATTから電力をデバイスに供給します。

 

注意: FX3 PMODEラインがUSB ブート(Z11)として構成され、VBUSピンがUSBコネクタのVBUS信号に接続されていない場合、デバイスは列挙されません。この場合、USBブート以外のブートオプション用にPMODEラインを構成することを推奨します。

 

Labels  Other

Tags: fx3 self-powered vbatt vbus Add tags

0 Likes
IFX_Publisher2
Community Manager
Community Manager
Community Manager
25 likes received 1000 replies posted First like given

Hi,  Nino san,

Confirmed to receive this KBA.

Thank you for your contribution.

Thanks,
Bindu

0 Likes