cancel
Showing results for 
Search instead for 
Did you mean: 

Community Translations

MaMi_1205306
Honored Contributor

Dear Sirs and  Madams,

I would like to translate KBA82598, please confirm to my work.

Regards,

Masashi

0 Likes
2 Replies
JennaJo
Moderator
Moderator

Hi, Masashi-san

Confirm for the work.

Thanks

Jenna

Jenna Jo
0 Likes
MaMi_1205306
Honored Contributor

Jenna-san,

I translated KBA82598 into Japanese.
We would appreciate it if you could confirm.

Regards,
Masashi

/***************************************************************************/

EXTCLKIN (LVCMOS input) Requirement for CY24293 - KBA82598

CY24293のEXTCLKIN (LVCMOS input) 必要条件 - KBA82598                     

Version:

**

質問:

LVCMOS外部クロック入力がCY24293のEXTCLKINピンに接続されている場合、特別な要件はありますか?

回答:

CY24293の外部クロック入力の入力デューティサイクル要件は35%〜65%です。

VIH、VIL、CINなどのその他の入力仕様は、データシートで指定されています。

0 Likes
Top labels