Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Community Translation - EPXFIFOBCH/L Registers of FX2LP – KBA219002

Kenshow
Level 8
Level 8
50 solutions authored 25 solutions authored 10 solutions authored

Hi,               

I would like to translate KBA219002 into Japanese.

Please confirm to my work.

Thanks,

Kenshow

0 Likes
2 Replies
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hi, Kenshow-san

Confirm to work this KBA.

Thanks

Jenna

Jenna Jo
0 Likes

Hi Jenna-san,

                                

Japanese translation was over.
Please check below.

Original KBA:

EPXFIFOBCH/L Registers of FX2LP – KBA219002

Thanks.

Kenshow

==============================

タイトル: FX2LPのEPXFIFOBCH/Lレジスタ – KBA219002

バージョン:**

質問:

EPXFIFOBCHおよびEPXFIFOBCLレジスタには何が含まれており、どのように使用できますか?

回答:

EPXFIFOBCHおよびEPXFIFOBCLレジスタには、インターフェースドメインから受信したバイト数が含まれています。これを使用する1つの方法は、長い転送の最後に外部マスターから送信される短いパケットをコミットすることです。これを行うには、スレーブファームウェアのTD_Pollで次のコードスニペットを使用します。

if( (( EPXFIFOBCH<<8) | (EPXFIFOBCL)) < 0x200) //if the packet is short(here x is the IN endpoint which //receives data from external master)

{

SYNCDELAY;

EPXFIFOCFG = 0x00; //change from Auto mode to Manual mode

SYNCDELAY;

INPKTEND = 0x0X; //commit the short packet

SYNCDELAY;

EPXFIFOCFG = 0x0C; //back to Auto mode

SYNCDELAY;

}

ここでは、ショートパケットをコミットするために、FIFO構成が自動モードから手動モードに変更されます。その後、マスターが長時間の転送を続行すると、自動モードに変換されます。

==============================

10-August-2020

  Kenshow