Community Translation - Differences between PSoC 4100S Plus and PSoC 4100S Family of Devices - KBA222580

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Kenshow
Level 8
Level 8
Distributor - Marubun (Japan)
50 solutions authored 25 solutions authored 10 solutions authored

Hi,

I would like to translate KBA222580 into Japanese.

Thanks,

Kenshow

Original KBA: KBA222580

Differences between PSoC 4100S Plus and PSoC 4100S Family of Devices

Translated by Kenshow

==============================

タイトル: PSoC 4100S PlusとPSoC 4100Sデバイスファミリの違い-KBA222580

バージョン:*A

質問:

PSoC® 4100S Plus PSoC 4100S ファミリ間のデバイスの違いは?

回答:

PSoC 4100S Plusファミリのデバイスは、PSoC 4100Sデバイスと比較して、より大きなフラッシュメモリ、より多くのペリフェラル、より多くのI/Oを提供しております。違いの詳細なリストについては、表1-1を参照してください。

  1-1 PSoC 4100SPSoC 4100S Plusデバイスの違い

特徴

PSoC 4100S

PSoC 4100S Plus

フラッシュ

64 KB

128 KB

SRAM

8 KB

16 KB

DMA

利用不可

8チャンネル

GPIO(最大)

36

57

スマートIO

2ポート

3ポート

タイマ、カウンタ、PWMTCPWM

5

8

シリアル通信ブロック(SCB

3

5

ECO + PLL

利用不可

利用可能


外付けの433 MHz水晶発振器(ECO)をサポートします。IMOECO、外部クロック、PLLから選択し、最大48 MHzの高周波クロック(HFCLK)も使用できます。

==============================

10-Apr-2020

Kenshow

0 Likes
1 Reply
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello, Kenshow-san

We receive your translation, it will be published to KBA to Community.

It will be reviewed internally.

After upload, You will receive the points as the word of KBA.

Due to the current volume of works, Please bear with me for the delayed the response.

It could be delayed, but it will be processed soon.

Thanks for your contribution to CDC!

Will keep you update the status.

Thanks,

Jenna Jo

Jenna Jo