Community Translation - Cypress's S71GL-N datasheet indicates 3.0V only and Vcc range of 2.0V to 3.3V. Which is the correct Vcc value? - KBA203370

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
KaKi_1384211
Level 6
Level 6
100 replies posted 50 replies posted 50 questions asked

Hi Jenna-san,

I want to translate the following KBA203370 into Japanese, please confirm to my work.

Cypress's S71GL-N datasheet indicates 3.0V only and Vcc range of 2.0V to 3.3V. Which is the correct ...

Thanks and regards,

Kiku

0 Likes
2 Replies
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hi, Kiku-san

Sorry for late response.

Confirm to work this KBA.

Thanks

Jenna

Jenna Jo
0 Likes

Hi Jenna-san,

Thank you for your confirmation

I have translated the following KBA203370 to Japanese.

Cypress's S71GL-N datasheet indicates 3.0V only and Vcc range of 2.0V to 3.3V. Which is the correct ...

_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/

【タイトル】

Cypress S71GL-NVCCについて - KBA203370

【質問】

Cypress S71GL-Nのデータシートに記載されているVCC3.0Vのみと2.0V3.3Vの範囲を示しています。

正しいVCCの値はどちらですか?

【回答】

Cypress S29GL-NのデータシートはコアVCC範囲が2.7V3.3V、及び 3.0Vのみの製品があることを示しています。

一般にデータシートのコアVCC範囲として2.7V3.6VのコアVCC範囲を持つCypress Flash Memory3.0Vデバイスとして

見なされ、注文部品番号(OPN) の「R」の指定がされない限り、3.0V範囲で動作します。

R」を指定されたFlash Memory3.0V範囲を指定しますが、コアVCC範囲は3.0V3.6Vです。

Flash Memoryは指定されたtACCの仕様を保証するために、3.0V3.6Vに『調整された』コアVCC範囲内で動作させる必要があります。

S71GL064NxxS71GL032Nxxは、どちらも3.0V範囲(2.7V3.3V)内で動作します。

_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/

Thanks and regards,

Kiku

0 Likes