cancel
Showing results for 
Search instead for 
Did you mean: 

Community Translations

KaKi_1384211
Honored Contributor

Hi,

I want to translate the following KBA into Japanese, please confirm to my work.

Current (Idd) consumption at -40 and +85 degrees?

Thanks and regards,

Kiku

0 Likes
2 Replies
JennaJo
Moderator
Moderator

Hi, Kiku-san

Confirm to work this KBA.

Thanks

Jenna

Jenna Jo
0 Likes
KaKi_1384211
Honored Contributor

Hi Jenna-san,

Thank you for your confirmation

I have translated the following KBA to Japanese.

Current (Idd) consumption at -40 and +85 degrees?

_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/

【タイトル】

周囲温度-40℃と+85℃の消費電流(Idd) について

【質問】

Memoryは周囲温度ー40℃と+85℃のどちらが最大消費電流(Idd) を費やしますか?

【回答】

Memoryは周囲温度+85(高温側) で最大の消費電流(Idd) を費やします。

_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/_/

Thanks and regards,

Kiku

0 Likes
Top labels