Community Translation - Comparison of features in PSoC™ 4100S devices - KBA232386

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
keni_4440091
Level 7
Level 7
500 replies posted 100 solutions authored 50 solutions authored

Dear supporter

I want to translate the following KBA. Please confirm to my work.

Comparison of features in PSoC™ 4100S devices - KBA232386

Regards,

Nino

0 Likes
6 Replies
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hi, Nino-san

Thank you for participating this activity.

Confirm to work this KBA.

Thanks, 

Jenna Jo
0 Likes

Dear Jenna

Somehow I can not find this article anymore. It seems this KBA is removed.

Please conform and let me know if I'm wrong.

Regards,

Nino

0 Likes

Dear Jenna

This is reminder for you. Thanks.

Regards,

Nino

0 Likes
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Dear Nino-san

Sorry that I missed your comment.

I think this Doc is not obsolete, but I also can't find it from Community.

I will contact internal team and get back to you.

Thanks

 

Jenna Jo
0 Likes
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hi, Nino-san

Would you proceed the translation work with published KBA?

https://community.infineon.com/t5/Knowledge-Base-Articles/Comparison-of-features-in-PSoC-4100S-devic...

It is now uploaded to community.

Thank you for your waiting.

Best regards, 

Jenna Jo
0 Likes

Dear Jenna

The following shows the translated version in Japanese for targeted KBA.

Please conform and double check.

Regards,

Nino

--------------------------------------------------------------------------------------------------

PSoC™ 4100Sデバイスの機能比較 – KBA232386

 

Version: *A

 

PSoC™ 4ファミリの最新デバイスであるPSoC 4100S Maxには、追加のflashメモリ、DMAチャネルがあり、I2Sブロック、暗号化アクセラレータ、高速I2Cなどの追加機能があります。

以下の表では、PSoC 4100S Maxデバイスの機能を、PSoC™ 4100S Plus およびPSoC™ 4100S Plus 256Kデバイスと比較しています。:

 

機能

PSoC™ 4100S Max デバイス

PSoC™ 4100S Plus デバイス

PSoC™ 4100S Plus 256K デバイス

CAPSENSE™

第5世代

第4世代

第4世代

Flash

384 KB

128 KB

 

256 KB

SRAM

32 KB

16 KB

 

32 KB

 

DMA エンジンのチャネル数

16 チャネル

8 チャネル

8 チャネル

暗号化

あり(AES, SHA, TRNG, PRNG, CRC 機能)

TRNG機能ブロックのみ

 

なし

I2S

あり

なし

なし

CAN

1つのCAN FDブロックで最大5 Mbpsまで動作

1つのCAN 2.0Bブロック

なし

I2C

高速、最大3.4 Mbpsまでをサポート

最大1 Mbps

最大1 Mbps

GPIO数

最大84本

最大54本

最大54本

Smart I/O数

24

24

16

 

: このknowledge base記事は、CAPSENSE™.に精通していることを前提としています。CAPSENSE™ アーキテクチャの詳細はGetting started with CAPSENSE™ およびCAPSENSE™ design guideを参照してください。

 

Labels   MCU & PSoC: PSoC 4  MCU & PSoC: PSoC 4 BLE

Tags: button capacitive capsense csd csd adc Fifth Generation Fourth Generation key keyboard keypad Moisture Tolerant mutual capacitance proximity psoc 4 psoc 4000s psoc 4100s PSoC 4100S MAX PSoC 4BLE Self-Capacitance sensing sliders smartsense touch touchpad trackpad User Interface Wake on approach water tolerance

0 Likes