Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

JuIn_1625121
Level 5
Level 5
100 sign-ins First solution authored 100 replies posted

original:Color Pattern FPGA Code Example to Test FX3 FPGA Interface - KBA229408

============================================

タイトル:

FX3とFPGAのインタフェースをテストするためのカラーパターンを出力するFPGAのコード例 - KBA229408

質問:

イメージ センサーを接続せずに、FX3 + ECP5 FPGA ベースの UVC カメラ設計のFPGA と FX3 のインターフェースをテストするにはどうすればよいですか?

回答:

FPGAとFX3のインターフェースのみをテストする場合、必要なフレーム解像度のサイズのカラーパターンをFPGAで生成してFX3に送信することができます。カラーパターンを生成するFPGAリファレンスプロジェクトは、このknowledge base articleに添付されています。FPGAマスターは、スレーブFIFOインターフェースを介して、1080pのビデオフレームを連続してFX3に送信します。KBA229407で入手可能なFX3ファームウェアを使用して、添付のFPGAプロジェクトをテストすることができます。

図1. FX3 + ECP5 FPGAベースのカメラ設計

Capture.JPG

このFPGAデザインには2つのモジュールが含まれています。1つ目のモジュールはフレーム解像度に基づいてカラーパターンを生成し、2つ目のモジュールは受信したデータをFX3に送信します(FX3 Master FIFOインターフェイスとして知られています)。FIFOモジュールは、バッファ1に1本の完全なラインを格納すると、FX3 Master FIFOインターフェイスに信号を送り出し、FX3にビデオデータを送信します。一方、FPGAは、FIFOバッファ2にビデオデータを格納することができます。同様に、FIFOバッファ2に1つの完全なラインがある場合、FX3マスターFIFOインターフェースに通知が送信されます。

カラーパターンは図2に類似したようになり、YUVフォーマットの1080pを60fpsでストリーミングします。カラーパターンのテストには、標準的なUVCホストアプリケーション(e-CAMViewなど)を使用することができます。

図 2. UYVY 1920 x 1080 @60 fps のカラーパターンpastedImage_22.png

UARTデバッグプリントを使って、フレームレートとフレームサイズがストリーミング解像度と一致していることを確認することができます。図3は、1080p UYVYが60fpsでストリーミングしている場合のデバッグプリントを示しています。DMAプロデューサイベントの数、コンシューマイベントの数、last partialバッファサイズ、完全なフレームサイズ、フレームレートが UART 経由で印刷されています。

図 3. フレームサイズとフレームレートのデバッグプリント

pastedImage_27.png

1 Reply
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello,

We receive your translation, it will be published to KBA to Community.

After upload, You will receive the points as the word of KBA.

Due to the current delay of internal review, Please bear with me for the delayed the response.

It could be delayed, but it will be processed soon.

Thanks for your contribution to CDC!

Will keep you update the status.

Thanks,

Jenna Jo

Jenna Jo
0 Likes