Original KBA:
Addressing Multiple CY8C201XX CapSense Express™ Devices on the Same I2C Bus – KBA221410
Translated by Kenshow
==============================
タイトル:同じI2Cバス上の複数のCY8C201XX CapSense Express™デバイスのアドレス指定– KBA221410
質問:同じI2Cバス上で複数のCapSense Expressデバイスをアドレッシングする方法は?
回答:
デフォルトでは、capsense Express容量コントローラーのI2Cアドレスはすべて0x00hに設定されています。カスタマーボードに2つのcapsense expressのパーツが必要な場合、マスターはI2Cバスのデータ破損を回避するために以下の手順に従う必要があります。
ステップ#1: マスターはXRESピンをhighにすることによりCE#1をリセットモードにします
ステップ#2: マスターはCE#2のコンフィグレーションファイル(PSoC Designerによって生成)をI2Cバス経由で送信します。PSoC DesignerでCE#1とCE#2に異なるアドレスを選択して、アドレスの競合を回避する必要があります。
ステップ#3: マスターがCE#2をリセットします(ソフトウェアリセットまたはハードウェアリセット)。
ステップ#4: マスターがXRESピンをHighにしてCE#2をリセットモードにします。ステップ#3の後、CE#2のアドレスが更新されるため、このステップはオプションになります。 0x00hからユーザー設定値まで。
ステップ#5: マスターはI2Cバスを介してCE#1のコンフィグレーションファイル(PSoC Designerによって生成)を送信します。
ステップ#6: マスターがCE#1をリセットします(ソフトウェアリセットまたはハードウェアリセット)。
注:
i) CE#1-「Capsense Express」のデバイス#1を指します
ii) CE#2-「Capsense Express」のバイス#2を指します
iii) 上記の手順が機能するためには、ボード上の少なくとも(2つのうち)1つのcapsense expressパーツがXRESピンにボンディングされていることを確認してください。
==============================
8-May-2020
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello, Kenshow-san
We receive your translation, it will be published to KBA to Community.
After upload, You will receive the points as the word of KBA.
Due to the current delay of internal review, Please bear with me for the delayed the response.
It could be delayed, but it will be processed soon.
Thanks for your contribution to CDC!
Will keep you update the status.
Thanks,
Jenna Jo