Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Community Translation - Address Large SRAMs using GPIF2 State Machine – KBA225268

Kenshow
Level 8
Level 8
50 solutions authored 25 solutions authored 10 solutions authored

Hi,               

I would like to translate KBA225268 into Japanese.

Please confirm to my work.

Thanks,

Kenshow

0 Likes
2 Replies
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hi, Kenshow-san

Confirm to work this KBA.

Thanks,

Jenna

Jenna Jo
0 Likes

Hi Jenna-san,

                                

Japanese translation was over.
Please check below.

Original KBA:

Address Large SRAMs using GPIF2 State Machine – KBA225268

Thanks.

Kenshow

==============================

タイトル: GPIF2ステートマシンを使用した大規模SRAMのアドレス指定 – KBA225268

バージョン:**

質問:cyfxsrammasterファームウェアサンプルのGPIF2ステートマシンを変更して、22本のアドレスラインでSRAMをアドレス指定するにはどうすればよいでしょうか?

回答:FX3SDKに付属するデフォルトのファームウェアサンプルcyfxsrammasterは、最大1KB2 ^ 8 * 32ビット)のメモリしかアドレス指定できません。このファームウェアは、LD_ADDR_COUNTを使用して、ステートマシンによってすでに読み取られたアドレス位置を追跡します。現在のデザインはより少ないメモリ(1KBのみ)を使用しているため、SRAM全体が読み込まれ、FX3バッファに保存されます。

GPIFステートマシンを変更して、22本のアドレスライン(2 ^ 22 * 32ビット= 16 MB)でSRAMをアドレス指定できます。2つのスレッド(TH0TH1)を使用して、1 KBのメモリチャンクを交互に読み取り、コミットします。両方のカウンター(LD_ADDR_COUNTおよびLD_DATA_COUNT)を使用して、アドレスの場所を追跡します。LD_ADDR_COUNT2 ^ 22に設定され、SRAMメモリ全体を追跡しますが、LD_DATA_COUNT255に設定され、1KBメモリを追跡します。1は、SRAMを読み取るためのGPIF2 SMのスニペットを示しています。1は、大きなSRAMを読み取るためのGPIF2 SMのフロー図です。

1. 大規模なSRAMにアクセスするためのGPIFステートマシンのフロー図

   Untitled.png

==============================

23-June-2020

Kenshow

0 Likes