Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Community Translation - 16-MHz BLE ECO for PSoC 6 BLE Demo Project – KBA223251

Kenshow
Level 8
Level 8
50 solutions authored 25 solutions authored 10 solutions authored

Hi,

I would like to translate KBA223251 into Japanese.

Thanks,

Kenshow

0 Likes
2 Replies
Kenshow
Level 8
Level 8
50 solutions authored 25 solutions authored 10 solutions authored

Original KBA:

16-MHz BLE ECO for PSoC 6 BLE Demo Project – KBA223251

Translated by Kenshow

==============================

タイトル:PSoC®6 デモプロジェクト用の16-MHz BLE ECO – KBA210620

バージョン:*A

質問:

PSoC 6 BLEデモプロジェクトを変更して、BLEに16 MHz ECOを使用するにはどうすればよいですか?

回答:

16 MHz ECOを受け入れるには、PSoC Creator / ModusToolboxプロジェクトのクロック構成を変更する必要があります。デモプロジェクトはデフォルトで、32 MHz ECOを使用するCY8CKIT-062-BLEキットを使用します。

1. デモプロジェクトを開きます。たとえば、「FindMe」プロジェクトを開きます。

2. [ Clocks ]をダブルクリックし、[ System ECO ] を選択します。

3. [ Edit Clock]クリックします。

pastedImage_5.png

pastedImage_0.png

4. Configure System Clocksウィンドウで、AltHF:BLE ECOオプションを有効にし、ECO周波数を16 MHz選択します。目的の分周器を選択するか、デフォルトを使用します。起動時間は、ECOクリスタルのデータシートで指定されています。負荷コンデンサは、ECOの周波数偏差を調整するために使用できます。詳細については、AN95089を参照してください。

pastedImage_10.png

ModusToolboxプロジェクトの場合、以下の手順を実行します。

  1. デモプロジェクトを開きます。たとえば、「FindMe」プロジェクトを開きます。
  2. Device Configurator-> Platformと移動し、ALTHFオプションをイネーブルにします。
  3. ALTHF - Parameters ウィンドウの中で、ECO周波数16 MHzを選んでください。目的の分周器を選択するか、デフォルトを使用します。起動時間は、ECOクリスタルのデータシートで指定されています。負荷コンデンサは、ECOの周波数偏差を調整するために使用できます。詳細については、AN95089を参照してください。

pastedImage_25.png

==============================

1-May-2020

Kenshow

JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello, Kenshow-san

We receive your translation, it will be published to KBA to Community.

After upload, You will receive the points as the word of KBA.

Due to the current delay of processed work, Please bear with me for the delayed the response.

It could be delayed, but it will be processed soon.

Thanks for your contribution to CDC!

Will keep you update the status.

Thanks,

Jenna Jo

Jenna Jo
0 Likes
This widget could not be displayed.