Original KBA:
16-MHz BLE ECO for PSoC 6 BLE Demo Project – KBA223251
Translated by Kenshow
==============================
タイトル:PSoC®6 デモプロジェクト用の16-MHz BLE ECO – KBA210620
バージョン:*A
質問:
PSoC 6 BLEデモプロジェクトを変更して、BLEに16 MHz ECOを使用するにはどうすればよいですか?
回答:
16 MHz ECOを受け入れるには、PSoC Creator / ModusToolboxプロジェクトのクロック構成を変更する必要があります。デモプロジェクトはデフォルトで、32 MHz ECOを使用するCY8CKIT-062-BLEキットを使用します。
1. デモプロジェクトを開きます。たとえば、「FindMe」プロジェクトを開きます。
2. [ Clocks ]をダブルクリックし、[ System ECO ] を選択します。
3. [ Edit Clock]をクリックします。
4. Configure System Clocksウィンドウで、AltHF:BLE ECOオプションを有効にし、ECO周波数を16 MHzに選択します。目的の分周器を選択するか、デフォルトを使用します。起動時間は、ECOクリスタルのデータシートで指定されています。負荷コンデンサは、ECOの周波数偏差を調整するために使用できます。詳細については、AN95089を参照してください。
ModusToolboxプロジェクトの場合、以下の手順を実行します。
- デモプロジェクトを開きます。たとえば、「FindMe」プロジェクトを開きます。
- Device Configurator-> Platformと移動し、ALTHFオプションをイネーブルにします。
- ALTHF - Parameters ウィンドウの中で、ECO周波数16 MHzを選んでください。目的の分周器を選択するか、デフォルトを使用します。起動時間は、ECOクリスタルのデータシートで指定されています。負荷コンデンサは、ECOの周波数偏差を調整するために使用できます。詳細については、AN95089を参照してください。
==============================
1-May-2020
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello, Kenshow-san
We receive your translation, it will be published to KBA to Community.
After upload, You will receive the points as the word of KBA.
Due to the current delay of processed work, Please bear with me for the delayed the response.
It could be delayed, but it will be processed soon.
Thanks for your contribution to CDC!
Will keep you update the status.
Thanks,
Jenna Jo