Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello, Contributors

2020 Autumn translation program is starting from Sep 1th.

For your work for KBA - below 50 candidate list is prepared.

Would you pick one of below KBA - and create new thread to claim your work?

Thank you for your continuous participation to Community.

If you have any question, please response to this Thread.

2020.09.07 Open/Claimed status update

KBA titleKBA addressStatus
FX3/CX3: UVC Extension Unit Application – KBA230466https://community.cypress.com/docs/DOC-20179Open
Relationship Between ICU Pins on Package and Internal ICU Channels in S6J3360 - KBA230042https://community.cypress.com/docs/DOC-19438Claimed
USB-Serial: UART Flow Control under CDC - KBA230578https://community.cypress.com/docs/DOC-20178Claimed
Use SFDP Data to Set Timeout Timer Value for SPI NOR Flash Page Program and Erase Operations - KBA230621https://community.cypress.com/docs/DOC-20041Claimed
Lattice Crosslink FPGA configuration and UVC Color bar video streaming using Cypress FX2LP – KBA30768https://community.cypress.com/docs/DOC-20048Open
USB2.0 Camera Interface Using FX2LP™ and Lattice CrossLink FPGA - KBA222479https://community.cypress.com/docs/DOC-14406Claimed
USB-to-Parallel Converter Using EZ-USB® FX2LP™ – KBA88219https://community.cypress.com/docs/DOC-10934Claimed
USB to Parallel Converter Using FX2LPhttps://community.cypress.com/docs/DOC-12251Claimed
Choosing between GPIF and Slave FIFO modeshttps://community.cypress.com/docs/DOC-11881Claimed
Difference between FX2LP™ Port I/O, GPIF, and Slave FIFO Modes - KBA83522https://community.cypress.com/docs/DOC-10998Claimed
LRD/SLWR  Pins During GPIF Mode of FX2LPhttps://community.cypress.com/docs/DOC-11732Open
Debugging when DMA Flags do not Work as Expected while Reading Data from FX3 – KBA230545https://community.cypress.com/docs/DOC-20201Claimed
Creating Custom BSPs in ModusToolbox - KBA230822https://community.cypress.com/docs/DOC-20725Claimed
Software Support for PSoC 64 Engineering Samples – KBA230748https://community.cypress.com/docs/DOC-20204Claimed
Placing the Wi-Fi Firmware Into External Flash in an AnyCloud Application - KBA230802https://community.cypress.com/docs/DOC-20696Claimed
elationship Between ICU Pins on Package and Internal ICU Channels in S6J3360 - KBA230042https://community.cypress.com/docs/DOC-19438Claimed
Swapping the Polarity on USB 3.0 Differential Pairs - KBA86900https://community.cypress.com/docs/DOC-10993Claimed
USB Differential Pair Pin Inversion - KBA218753https://community.cypress.com/docs/DOC-10504Claimed
MoBL SRAM Definitionhttps://community.cypress.com/docs/DOC-9718Claimed
S6BP501A/502A PMIC Under Cold-Cranking Conditions – KBA223770https://community.cypress.com/docs/DOC-15087Claimed
Byte Power Down feature in MoBL SRAMshttps://community.cypress.com/docs/DOC-11493Claimed
Flash Memory Consumption of Various Features Available in CCG3PA Based Power Bank Project of CCGx Power SDK 3.2 - KBA224248https://community.cypress.com/docs/DOC-15295Claimed
Serial Wire Debug (SWD) Using USBIO Pins in PSoC® 3 and PSoC 5LP – KBA82881https://community.cypress.com/docs/DOC-11978Claimed
Design and Programming Checklist for for PSoC® 3/ PSoC 5LP – KBA208166https://community.cypress.com/docs/DOC-9294Claimed
Wrong ADC Macro Names Used in adc.c in PDL 2.1.0 - KBA228999https://community.cypress.com/docs/DOC-18625Claimed
Wrong Register Access SCIS01 and SCIS23 in adc.c in PDL 2.1.0 - KBA229088https://community.cypress.com/docs/DOC-18677Claimed
PCM Sound Source Input in Traveo S6J3200 Series MCUs - KBA226513https://community.cypress.com/docs/DOC-16872Claimed
New code compressor directives in Imagecraft compilerhttps://community.cypress.com/docs/DOC-12504Claimed
ImageCraft code size optimizationhttps://community.cypress.com/docs/DOC-9810Open
Linking External C Files to a PSoC Designer Project with Imagecraft Compilerhttps://community.cypress.com/docs/DOC-11534Claimed
Getting an Internal Inconsistency Check Error - KBA92909https://community.cypress.com/docs/DOC-10840Claimed
Build error in PSoC Designer 5.0 on a German or French Operating Systemhttps://community.cypress.com/docs/DOC-12188Claimed
Warning: Machine Instructions Inside .LITERAL/.ENDLITERAL Labels - KBA83511https://community.cypress.com/docs/DOC-11066Claimed
“Old Style Function Definition" Warning in PSoC® Designer™ - KBA83779https://community.cypress.com/docs/DOC-12051Claimed
Switching Between ImageCraft™ and Hi-Tech C® Compilers – KBA83349https://community.cypress.com/docs/DOC-11008Claimed
Building PSoC® Creator™ Projects Using Commands - KBA88205https://community.cypress.com/docs/DOC-10865Claimed
CyUSB.sys Support For WinServer 2003https://community.cypress.com/docs/DOC-9828Claimed
Editing Firmware Constants Using Compiler Arguments in PSoC® Creator™ - KBA213561https://community.cypress.com/docs/DOC-10584Claimed
Display a Long on LCDhttps://community.cypress.com/docs/DOC-12305Claimed
Free C Compiler for PSoC Designerhttps://community.cypress.com/docs/DOC-12307Claimed
Documentation and Training for PSoC® Creator™ Component Development - KBA80958https://community.cypress.com/docs/DOC-11408Claimed
Basics of Verilog and datapath configuration tool for component creationhttps://community.cypress.com/docs/DOC-11409Claimed
Configuring CapSense Express devices through PSoC Designer 5.1https://community.cypress.com/docs/DOC-12236Claimed
Unable to see any blocks in chip editor window : Chip editor is blank in PSoC Designerhttps://community.cypress.com/docs/DOC-11340Claimed
PSoC® 3, PSoC 4, and PSoC 5LP AN Project File Naming Convention and Use – KBA84803https://community.cypress.com/docs/DOC-12335Claimed
Building a PSoC® Creator™ Project from the Command Prompt – KBA88169https://community.cypress.com/docs/DOC-10957Claimed
Creating and Configuring Command Shortcut Keys in PSoC® Creator™ - KBA90934https://community.cypress.com/docs/DOC-10963Claimed
Displaying a Float Value on LCD Using PSoC® 3 or PSoC 5LP – KBA94460https://community.cypress.com/docs/DOC-12439Claimed

Thanks,

Jenna Jo

Jenna Jo
0 Replies