Community Information Forum Discussions
Are there vacant positions for dual bwl studies in Munich this year?
Please move this thread from forum PSoC4 to forum PSoc5
https://community.infineon.com/t5/PSoC-4/accuracy-of-adc/td-p/404308
Show LessHi guys, not sure where to place this thread.
I'm a new member and have been contacted by scammers in PM already (user @revfrancis1 ). It appears you have a problem with scam accounts. See below for the message I recieved:
With respect, please permit me to inform you of my desire of going into good business relationship with you, originally I am a supervisor to a gold mining union here, nonetheless now we are strangers to ourselves reason you have to contact my private email address (jesusislord956@gmail.com)
For more detail most important to know you better,
I am Rev Francis Adam one of my important purchaser deposited money in one financial bank here to trade on gold, unfortunately he dies recently and I was his next of kin to that money, I will need your sincere assistance to serve as a guidance to this fund so you can easily and officially help me receive this money in your country after knowing you better understand, I am sincerely willing to offer you 25% of the total amount as compensation for your help and sincerity, More important we have genuine Gold here, your friends, business associates or brother if interested can contact me directly through you, Our details Product Specification
Product.....Gold Dory Bars
Quantity..........150 kg
purity......95.6 %
carats......23 plus
Price.......... per Kg to be negotiated
Thanks and God bless you and your family Amen.
Rev. Francis .Adam
There are some scammers in the forum sending private messages. See, for example this thread
The messages are sent by the user 'revfrancis1' and is an apparent scam
Show LessSeveral years ago I designed in ESD0P2RF-02LRH diodes for ESD protection. They went EOL. I switched to ESD112B102ELE6327XTMA1. Now those parts are marked NRND. Is there a substitute available? Any idea if it'll be in production for more than a couple of years? It's frustrating to constantly be updating my designs because a simple ESD diode is no longer available.
Show Less
The search engine is not working on several forum threafds. For example, attempting searching for "UART" in "Microcontrollers" or "PSoC4"produces valid pool of results (Screenshot 1), but performing same search in "PSoC5" or "Code examples" returns no results (Screenshot 2).
Tested using Android and Chrome (Win 11)
Screenshot 1.
Screenshot 2
Show Less
Dear Supplier,
I am from Environmental team of Thales India, who is contacting for environmental information.
Attached is the declaration from INFINEON for non-inclusion of substances-of-concern.
As per the statement it seems like there could be presence of Ozone Depleting Substances (ODS) up to 1000 PPM.
Please specify the Ozone Depleting Substances if at all present in your products at any concentration.
Thank you in advance for your fast reply.
Best regards,
Vishwajith M
Senior Engineer - Environmental and Chemical Data
Thales India Engineering Centre
Show LessHello Team,
Within the framework of the Lead (PB) Analysis activities for the components of THALES equipment's or products, and in order to update our databases,
I would like to know about the presence of lead in the component for the Infineon (International Rectifier) of below part numbers.
30FQ045
540
IRFF130
2N6796
IRFF9120
IRC530 (OBS)
IRFF9220 I
IRFF230
If Material declaration form available (to calculate the lead presence), Kindly provide for the attached parts.
If there are errors in codification with respect to references "Part Number", please indicate the exact one.
Thank you in advance for your quick response.
Regards,
Prasanna.
Show LessDear community
I have a question regarding the HyperBus Controller which we originally got from Spansion. We used this IP succesfully in our Xilinx Kintex and Artix 7-Series devices. We face now problem when we use the IP in a Xilinx Ultrascale architecture.
The problem concerns the RWDS IO signal.
The output signals from the IP are wds0, wds1 and wds_en. They are synchronized first and then led to an output DDR FF which is connected to the RWDS output buffer.
According to the specification, the input buffer of the RWDS signal is on one hand connected to the IP and on the other delayed and connected to a clock Buffer.
The implementation of this structure yields errors and in the documentation of Xilinx I have found that clocks should not be delayed using delay elements as they cannot be directly routed to global clock buffers. They recommend instead to use an MMCM or a PLL. As this signal is a strobe rather than a clock, using such elements is not feasible either.
Is there an updated version of this IP which supports Xilinx Ultrascale architecture or was someone succesfull in using this IP in an ultrascale environment
Thank you very much in advance for your answers
Show Less