Community Information Forum Discussions
Hi,
I see there have been changes made to the forum.
Where is the "Code Examples" subforum?
I see that the "Blogs" now have two references. One at the top menu and the other in "Resources/Blogs".
I see that the "Training" now have two references. One at the top menu and the other in "Resources/Training".
I also see that "Projects" has moved to "Resources/Projects".
"Community Information" has now been moved under "About"
If you're going to put back "Code Examples" I would at a minimum suggest placing it under "Resources". However, I'd better recommend that a "Code Examples" subforum be added under each product subforum in "Forums". And that all the previous examples be sorted as to the product that the code examples that apply. This allows for better filtering of applicable examples for the users' area of interest.
Show Lesscould you please answer the following question we received via social media?
Question: Will these SSR be having micro leakage?
Link to the post: https://www.facebook.com/345383962211058/posts/6257172827698779/
Thank you!
Show LessPlease unlock the thread
Building a 16-bit PWM DAC out of 8-bit Fractional PWM and DeltaSigma Modulator
Show LessTrying to find Infineon cross to the following parts:
LTC4365ITS8#TRMPBF |
IC, OV, UV, AND RVS SPLY PROT CONT, TSOT-23, ROHS |
LTC4365ITS8-1#TRMPBF |
IC, OV, UV, AND RVS SPLY PROT CONT, TSOT-23, ROHS |
MAX6354LSUK+ |
IC, DUAL-VOLT UP SUPV CKTS, SOT-23, ROHS |
MAX16030TG+ |
IC, QUAD-VOLT, CAP-ADJ, SEQ/SUPV CKTS, TQFN-24, ROHS |
ADP7105ARDZ-3.3 |
IC, 20V, 500MA, LOW NOISE LDO RGLTR, SOIC-8, ROHS |
Who can correct this error with the Cross Reference database?
Searching for a cross to
- TI’s TPS65987DDHRSHR USB Type-C® and USB PD controller with integrated power switches
Infineon’s Cross Reference returns
- Infineon’s IR35221 Digital Multi-phase Controller 8-phase Dual Loop PWM Voltage Regulator Quality Requirement Category: Industrial
Show Less
Hi,
I see there is a "User Group" called "InfineonSpice Desktop Circuit Simulator".
Is there plans to release an Infineon supported Spice simulator?
Show LessThe new "Projects" SubForum is no longer accessible.
I have requested for some technical information. They said they will give me access to myICP home page where i can find technical data. I got access to home page. But there are no sites available in that home page. I kindly request you to provide the access for the sites.
Show Less之前登录infineon nextcloud需要用pinid输入一次性密码,后来把app卸载了,再重装app之后要求手机配对设备,需要输入配对秘钥,请问要怎么重新配对?