Community Information Forum Discussions
Is the MB3761PF-E1, which was transferred from Fujitsu to Spantion in 2013, the same as the MB3761PF-EFE1?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E3%82%B3%E3%83%9F%E3%83%A5%E3%83%8B%E3%83%86%E3%82%A3%E6%83%85%E5%A0%B1/%E5%90%8C%E7%AD%89%E5%93%81%E3%81%8B%E3%81%94%E7%A2%BA%E8%AA%8D%E3%82%92%E3%81%8A%E9%A1%98%E3%81%84%E8%87%B4%E3%81%97%E3%81%BE%E3%81%99/td-p/686844
Show LessWhen editing forum post that includes a code section, I noticed that the spacing around the code automatically increments +1 space line after each editing (see picture below). It is possible to manually delete the spacing during editing, but at least one line before and after will be automatically inserted after the edit anyways.
As a non-native speaker, I edit message text heavily, and the extra spacing keeps growing and growing....
Figure 1: The Yellow markup shows the spacing, which automatically grows in size after each edit attempt
Show Less
Hello.
Can you unpin the message in PSoC4 forum:
Solved: modustoolbox的capsense键值获取 - Infineon Developer Community
I don't know why it was pinned.
Thank you.
Show LessPlease move this Traveo-related question
How to implement the TCPWM Quadrature Decoder Mode
from the Code Examples to the corresponding forum TRAVEO™ T2G Forum Discussions
Show Lesssmartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%A4%BE%E5%8C%BA%E4%BF%A1%E6%81%AF/I-have-two-questions-about-the-use-of-20719-classic-Bluetooth-could-someone/td-p/681370
Show LessHello.
Please delete spam message from this thread:
PSoC 5LP unable to fit configuration in 24 UDBs - Infineon Developer Community
and from this thread:
Re: XDPP1100 PWM duty resolution - Infineon Developer Community
from user : thekbhgames
https://community.infineon.com/t5/user/viewprofilepage/user-id/162236
regards.
Show LessI now have the LTE 9832 and need to download the program, what tools do I need to prepare, software interface hardware,
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%A4%BE%E5%8C%BA%E4%BF%A1%E6%81%AF/%E8%80%81%E4%BA%A7%E5%93%81%E7%9A%84%E9%97%AE%E9%A2%98/td-p/656370
Show LessHi, Indfineon team
Could you please provide the Land-patterm for S80KS2564GACHB043 (PG-BGA-49-800) asap?
This is Customer Requirement.
Regards,
Muro
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E3%82%B3%E3%83%9F%E3%83%A5%E3%83%8B%E3%83%86%E3%82%A3%E6%83%85%E5%A0%B1/S80KS2564GACHB043-Land-Pattern-PG-BGA-49-800/td-p/480855
Show LessI made a post in the Power Management forum and it apparently is marked as spam? I submitted an abuse report to the moderator to change it but haven't heard back. How can I fix this?
Show Less