Community Information Forum Discussions
text.format{('custom.tabs.no.results')}
Can anyone give the support for how to use TPM for storing the secure boot keys in imx6/imx8 series platforms. All the suggestions are highly appreciated. Show Less
I use the TLI4970050 MS2GO evaluation board, with the Current2go software GUI
I tried to change the OVCL.
I connected GND to my GND Power Supply,
then connected the P pin to 20.60V
then clicked on Burn into EEPROM.
Unfornately it failed, and put all byte of the EEPROM to FF.
Do you know the detailed procedure ton program the EEPROM with Curent2go software ?
Thank you
Etienne TH Show Less
Hello!
The target is to run tests in 2 browsers, the test script should be modified. What was done: if (Cypress.isBrowser('chrome') & Cypress.isBrowser('firefox')), as results test is running, but in default browser, what is electron or it depends what is selected browser in cypress runner. I have 3 browsers now. I did ./node_modules/.bin/cypress run --browser chrome this works, but unfortunately looks like it's impossible to ./node_modules/.bin/cypress run --browser chrome and ./node_modules/.bin/cypress run --browser Firefox. Also I added script in package .json file - "cypress-multi-browsers": "npm run unified-cypress-dev -- --browser firefox & npm run unified-cypress-dev -- --browser chrome", but getting errors about Firefox security.
Any suggestions?
Many thanks )
Show Less
i am planning to use Bgb707l7esd in my project for satellite receiver.
i have below query regarding this part number.
As per the layer stacking information given from your end, we have below query.
As layer stack up shows in application note (https://www.infineon.com/cms/en/product/rf-wireless-control/low-noise-amplifier-lna-ics/general-purpose-lnas/bgb707l7esd/#!documents) that it has top layer of rogers and bottom layer of FR4 for BGB707L7ESD,
I want to use FR4 as both layers. Is it possible or it will effect the performance?
Kindly request you to provide information as soon as possible.
Thanks Show Less
Exiting (backing out) a specific thread deposits you back at the first page of forum subtopic you entered from. This is annoying.
For example if enter a thread on page 7 of Home/ General/ Community Information and then back out from the thread, I'm returned to page 1 of Home/ General/ Community Information.
This can be considered annoying if you're trying to parse through the subtopic.
Show LessIn a post I inserted C code using the "Insert/Edit Code" feature and selecting "C"
The inserted text showed up with C format while in edit mode.
Once I posted it to the forum, the formatting was removed.
CY_ISR(ISR_SAW_GENERATOR) {
static uint8_t tbl_idx = 0;
PWM_UPDATE_INTERRUPT_REQ_REG = PWM_UPDATE_INTR_MASK_TC; // ClearInterrupt
uint32_t msb = saw[((tbl_idx++) & 127)];
UPDATE_DR |= UPDATE_MASK;
PWM_MSB_COMP_CAP_BUF_REG = msb; /* Load the Compare Buffer for the swap */
UPDATE_DR &= ~UPDATE_MASK;
}
It appears to work in the above example.
However check out my posting in this link: PSoC4-PWM-bug-Glitch-on-Compare-Reg-Write
Show LessHi,
In response to the previous (locked) thread
Test thread 6th Jan - Checking - making this title a big one to test how willi itappear by editing..
Please consider removing the title altogether in all posts as unnecessary. Adding title to every post looks odd, takes space and bears no information.
Show LessIn the following thread:
PSOC4 Power-on-reset problem - Cypress Developer Community
The 6th reply (user name "qwerty") looks like a weblink to a virus webpage.
Please investigate and delete the message before someone clicks on the link.
regards.
Show LessTell us what the output voltage is on the PXE11110-IR35412
The PXE1110 option is not stitched.
The PXE1110 version is stitched by the default firmware from the power code.
Подскажите какое выходное напряжение на связке PXE1110+IR35412
Вариант PXE1110 не прошита.
Вариант PXE1110 прошита прошивкой по умолчанию из power code. Show Less
Tell me the chips of the controller PXE1110 are sold stitched? Are they already wearing basic firmware?
For example, when buying here - https://ru.mouser.com/ProductDetail/Infineon-Technologies/PXE1110CDMG003XTMA1?qs=HXFqYaX1Q2zyfapwndJKcA%3D%3D
Подскажите микросхемы контроллера PXE1110 продаются прошитыми? В них уже сть базовая прошивка? Show Less