Community Information Forum Discussions
I keep posting questions or problems on this forum, they go unsolved, and then the topic is locked, even though it's still an unsolved problem. Sometimes a "solution" is even chosen for me that doesn't actually solve my problem. Why? It's frustrating. If it stayed open, we could continue putting notes and other people with the same problem could also comment, maybe finding a solution. But instead, everyone needs to create new topics about the same issue, not seeing each other's posts.
https://community.infineon.com/t5/PSoC-5-3-1/We-were-unable-to-find-the-symbol-There-are-several-things-that/m-p/280477 is still a problem, for instance.
Show LessHi,
I'm looking for a place to find LTB/LTS/EOL documents
I can see that TDA21241AUMA1 is discontinued on the website, but I thought it was NRND and haven't seen a PCN on it.
This has made me curious if there is a place where I could see this for all Infineon parts as it would be helpful with this case and in the future.
Thanks,
Ryan
Show LessHi,
It appears that links to the outside sources are no longer allowed, and posts with such links are permanently deleted. No draft version remains. This is quite sad, as some legitimate links, for example, to the supplementary YouTube demos are quite useful.
Another issue is that such posts are deleted entirely, not even a draft remains, forcing to manually re-type the entire post. Is it possible to keep at least a draft, so it can be edited and corrected if necessary?
Show LessHi,
Is it possible to unlock this discussion Stream output of Filter Channel A into Filter Channel B
/odissey1
Show LessHi,
It appears that clicking on custom images in the message body doesn't zoom images anymore. It results just in darkened screen. Used to work OK previously. Tested on Android 11 and Win10 (Explorer, Chrome).
/odissey1
Figure 1. Some test image (click me)
Show Less
Hi,
One of my customer wanted to browse PSoC 4 KBAs, so I suggested to visit here.
The customer could arrive at this KBA page, and he could even filter the topic for PSoC 4.
And it shows that there are 344 topics for PSoC 4.
But when trying to select page "2", suddenly there is "No Discussions"
Similarly selecting the next page ">" shows the same result
Would someone in charge of this page fix this?
moto
Show Less
I am not able to download CY8CKIT-062 design files or any files. I get a message:
The requested URL was rejected. Please consult with your administrator.
Your support ID is: 15752085814832961338
For example, this applies to the following URL's:
https://itools.infineon.com/archive/CY8CKIT062BLESetup_RevSE.exe
https://itools.infineon.com/archive/CY8CKIT-062-BLE%20PSoC%206%20BLE%20Pioneer%20Kit%20Firmware.zip
https://itools.infineon.com/archive/CY8CKIT062BLESetupOnlyPackage_RevSE.exe _
Infineon-CY8CKIT062BLESetup_RevSE.exe-DevelopmentTools-v01_00-EN.htm
Infineon-CY8CKIT-062-BLE_PSoC_6_BLE_Pioneer_Kit_Firmware.zip-DevelopmentTools-v01_00-EN.htm
Infineon-AIROC_CySmart_Bluetooth_LE_Test_Debug_Tool-DevelopmentTools-v01_00-EN.htm
Show Less
To the Moderator:
Please delete last post from AdamGreen in the discussion
PsOC4 Project - Alarm Loop - Infineon Developer Community
It is SPAM!!!
Show LessCan Physically apply Newton's III 3rd third law of motion, as a cycle system in a Motor Engine Device?
3rd Thermodynamic Law Applicated in a Power-Plant Device. The Reaction at From of the Action. New Torque Power. Its a simple Plus Formula of the Interaction of the Two Powers: 1/Action, + 2/Reaction = Retrodynamic. / For every action there is an equal and opposite reaction.
RETRODYNAMIC Effect - Dextrogiro => vs <= Levogiro Phenomena Effect. / Rotor/RPM VS InFlow/Way. 2dn Thermodynamic Law Applicated in a Power-Plant Device. The Reaction at From of the Action. New Torque Power. Its a simple Pluse Formula of the Interaction of the Two Powers: 1/Accion, + 2/Reaction = Retrodynamic.
"Changing rotation inside a mass makes it possible to change its inertial properties. It is the equation for a jet motion without rejection of any mass.” Albert Einstein.
The formula of the Retrodinamic effect is a simple mathematical summation. What is Dextrogiro plus Levogiro, gives the result of the sum, of what is the total, which is the retrodynamic effect. But keeps doing Exponential.
The logic of creation of an inertial propulsion system is thus: Any motion is rotation ---- Rotation of a matter generates a space-time Torsion ---Torsion of space - time is described by Ricci torsion --- Ricci torsion is an inertial field-----the rest mass of any object is determined by its inertial field---- operating by fields and forces of inertia inside of mass we can create inertial propulsion system which moves according to the equation [m (t) dv/dt =-vdm/dt].
Newton's Third Law of Motion: III. For every action there is an equal and opposite reaction.
It is the sum of both (two) Forces - one to other.
http://stateoftheartnovelinflowtech.blogspot.com
https://padlet.com/gearturbine/un2slbar3s94
https://www.behance.net/gearturbina61a
🤔🤡🤖😺
🌹👍👀👄
💣💎🐞🦋
Show Less