MOSFET (Si/SiC) Forum Discussions
text.format{('custom.tabs.no.results')}
Howdy y'all,
As the title implies, I was curious as to what the recommended torque was to secure the IPTC012N08NM5 to a heatsink? I couldn't find anything in the datasheet or any of the supplemental documentation on what the force should be.
Thanks
Show LessHello, I need to know the correct part number associated to ordering code SP005591068.
BTS409L1E3062AA or BTS409L1E3062AB ?
Thanks.
Best Regards
Show LessDear Infineon team,
the spice model of the IMZA120R014M1H and other models in the same .lib file are incompatible with SPICE.
In LTSPICE the program repots: "ERROR: Node U1:$M009F:$M01LF:N03D6 is floating and connected to current source G:U1:$M009F:$M01LF:01NW".
The VCCSs G01NW and G01O5 have specified 2 nodes and a value. A VCCS needs to be specified with 4 nodes, correct?
Is there a fix for this issue?
Hello,
IRFP044NPBF is discontinued, I found IRFP064NPBF, can I use it to replace the IRFP044NPBF ?
My project uses this mosfet as an electronic load for 20V, 3A, 60W max.
Show LessThere is said that this bright feet + logo a bit unlike is IR Mexico factory production, I can not judge, please gods look at, this is not authentic, thank you!
Show LessWhere are CAD models for QDPack.
There are .pdf files at https://www.infineon.com/cms/en/product/packages/PG-HDSOP/PG-HDSOP-22-1/ These are NOT CAD models.
STEP form would be preferred.
Greg
Show LessI am looking for a Power MOSFET. I need a Silicon (Si) transistor with high Vds >500V, but I don't know how to find the transistor I need. The list on the website doesn't state transistor material. Please help.
Show LessHI all, new to the forum so I apologize if this repeats similar posts.
I have a design that needs to switch high power to drive LEDs for short pulses.
The voltage to the LED string is 45V and the current is a maximum of 24A.
the pulsewidth is 5mS and the overall pulse-train frequency is 5 Hz.
I am looking at using the IAUZ40N06S5L050. this FET is at the bottom of the string and according to LTSpice sees only about 24V for Vds. So the question is, according to the datasheet, this is a bit outside of the safe zone but only slightly, I am restricted to very small space so the package/footprint is a good fit. Will this work?
Show Lesssmartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOSFET-Si-SiC/%E6%81%92%E6%B5%81%E6%BA%90%E9%A9%B1%E5%8A%A8/td-p/744186
Show LessHi :
I bought some IRFP90N20DPBF this PN, but after our QC inspection, parts with some mixed DATECODE inside.
Ifs that situation due to from IFX MFR side?
plz help advise here.
thx~
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOSFET-Si-SiC/About-IFX-MOS-parts-with-mixed-DATE-CODE/td-p/743754
Show Less