Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Code Examples Forum Discussions

Sort by:
NXTY_Tatebayasi
Code Examples
Hi,Community,   I created a project to start CAPSENSE Tuner with UART for PSoC4000S.The CAPSENSE project borrows from the proximity sensing project(CE225691... Show More
nguyenhuy
Code Examples

Hi guys, is there library or code example UART Rx for SP490. I found only example for UART Tx for Sp490. Thanks you

nguyenhuy
Code Examples

how can i declare NO_INIT  variables in SP490 sensor? 

Spartan2614
Code Examples
In SPI_DMA example how queue works for multiple slaves in single node , unable to understand from documents of iLLD.@User16286  Show More
Len_CONSULTRON
Code Examples
Hi, I've uploaded an example project that illustrates very efficient ISR coding of 11 UART Rx ports. It is uses a SW circular FIFO buffer for each por... Show More
Len_CONSULTRON
Code Examples
To all,I've enhanced some of my previously submitted code shares (Terminal Component - Simplifies UART or USBUART communication and GetString() function that supports input character filtering.  Includes menu-driven commands.... Show More
Len_CONSULTRON
Code Examples
UPDATED: 12.30.2021 Hi, I'm attaching a project which includes a pre-component version of a 14-bit VDAC using the dithering method to generate the ext... Show More
SaGa_4641021
Code Examples
Hi I am using a code example (CE218964 - PSoC 6 MCU RTC Daily Alarm). the printf() functions does not print to serial port. I had the same issue with ... Show More
seku_495601
Code Examples

Need Example Code for Simultanously 2 filter output with one output filter changable to LPF/BPF/HPF  in PSOC 5LP

R4mses
Code Examples
  Hola que tal Tengo un proyecto el cual ocupo comunicarme con el CY5677smart bluetooth low energy, ocupo leer, escribir datos. Alguna persona tendra ... Show More