Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Code Examples Forum Discussions

Sort by:
Translation_Bot
Code Examples
Description OverviewI wrote code to make a sound using the slider of the CY8CKIT-042 PSoC 4 Pioneer Kit.1. Get a position on the slider.2. Set the PWM... Show More
JJack
Code Examples
Dears, please find my solution for the calculation of the parity value for 32-bit data words in 64K SRAM blocks with 32-bit access attached. The code ... Show More
MotooTanaka
Code Examples
Hi, While ago, we had a discussion asking for charLCD sample for PSoC 6. https://community.cypress.com/t5/PSoC-6-MCU/Display-LCD-on-PSOC-6/m-p/266274... Show More
AdithyaS
Code Examples
This is  a code example which is used to interface the TLE5012B angle sensor in the TLE9879 board. This helps in receiving the angular information abo... Show More
NarraPugitha
Code Examples
The code example exemplify the possibility to connect multiple radar sensors with a specific UUID. This helps the user to evaluate the multiple radar ... Show More
Siddharth
Code Examples
Different radar configurations between set of frames are required to enable different kinds of measurements simultaneously. For example, To have a dif... Show More
odissey1
Code Examples
This is an example of the  8-bit PCM audio playback on PSoC4200M CY8CKIT-044 Pioneer Board using DMA. Unlike the previous example, which used an inte... Show More
odissey1
Code Examples
This is an example of the  8-bit PCM audio playback using PSoC4200M and CY8CKIT-044 Pioneer Board. Audio data are stored in the PSoC FLASH in 8-bit si... Show More
Geronimo
Code Examples
Hi, I am looking for the  CY3635 Wireless USB N:1 DVK hub/sensor firmware. I can only find the host software/docs below. I need the PSoC firmware i.e.... Show More
MotooTanaka
Code Examples
Hi, Here is my code sample of measuring a pin capacitance using the CapSense component.I used CY8CKIT-044 but I hope that porting this to ather PSoC 4... Show More