Code Examples Forum Discussions
Hi, Community,
Here is an example code to measure power consumption of PSoC4000S without entering low power modes like Deep Sleep. Please note that in order to perform the experiment, you will need to remove resistors R22 and R23 on the CY8CKIT-145 evaluation board.
And I removed the jumper on J3 and measured it using the current mode of a tester.
The system frequency of the PSoC4000S is set to 24MHz.
The result shows that the power consumption of the PSoC4000S, with VDD = 3.3V, is approximately 4.8mA.
Was my expectation that it would be about the same as IDD8 correct... ?
I attached the main.c file. Please add it to an empty project.
The TopDesign is as shown in the image.
Best Regards,
Chihiro Tatebayashi / NEXTY
This is an example of the 8-bit PCM audio playback on PSoC4200M CY8CKIT-044 Pioneer Board using Double-Buffered DMA.
Unlike the previous example, which used single-buffered DMA to update the IDAC8, this project is using a Double-Buffered DMA to transfer the data. This has several benefits, compared to previous example:
- No limitation on the audio data size.
- Possibility to mix data from several data sources or manipulate the data
- Seamless data output (no interruptions).
The drawback of the approach is certain processor load, which has to repeatedly populate the Buffer with fresh data. This load, however is much lower compared to using direct interrupt write without DMA.
The Double-Buffered DMA uses intermediate RAM Buffer of size 2N=64 bytes made of two equal halves, to store the data coming from the data source. The DMA1 consists of two chained Transfer Descriptors TD0 and TD1, which copy data byte-by-byte from the Buffer to the temporary RAM location (TMP). Once TD0 finishes copying the data from the first half of the Buffer, it chains to the TD1, which copies data from the second half of the Buffer and loops back to TD0. In this demo, the Buffer size is 64 bytes. Actual size should be set depending on the latencies of the processor, but 128+128 is typically a good size. Project dataflow:
Once TD0 (or TD1) is completed, an interrupt is fired, signaling that this Buffer half needs replenishment (while the other one is busy). At this point processor need to copy fresh portion of the data from the data source (here it is a FLASH), and wait for the next data request, while the Buffer content is being continuously played without interruption.
The data source can be RAM, FLASH, SD card, or processor generated data (sine, etc.).
To get the data to the IDAC8, the 8-bit data is first copied by DMA1 from the Buffer into intermediate (16-bit) location in RAM, where the MSB keeps IDAC control settings, and LSB has the data. The DMA2 then transfers 2 bytes {MSB, LSB} to the IDAC8 control register. Such intricate scheme is required because the DMA transfer to the IDAC is always 16-bit, thus the attempt to send only the data byte wipes off the IDAC control settings.
The project is configured to play on startup the Sawtooth test waveform in the continuous loop. Optionally, it can be configured to play a single time by enabling the SINGLE_SHOT directive.
The audio data are stored in the PSoC FLASH in 8-bit unsigned PCM format. Attached project includes several test PCM audio files in 8-bit unsigned format:
sawtooth_8-bit_S.h - test sawtooth, 8-bit, Unsigned (size= 256 bytes)
smb_world_clear_5k5_N_U.h - Super Mario theme, 5.512kHz, Normalized, Unsigned (size=33600 bytes)
smb_world_clear_11kHz_N_U.h - Super Mario theme, 11.025kHz, Normalized, Unsigned (size=65536 bytes)
smb_world_clear_22kHz_U.h - Super Mario theme, 22.05kHz, Unsigned (size=65535 bytes, clipped)
The WAV files have been converted to the C code using WAVtoCode v1.1.1 by Colin Seymour. The original WAV data have been Normalized to fill the entire 8-bit scale, which has increased the dynamic range.
Project attached contains all necessary files. It was tested using both Creator 4.0 and 4.4.
Credits:
WAVtoCode v1.1.1 by Colin Seymour: https://colinjs.com/software.htm#t_WAVToCode
Figure 1. Project schematic. The PCM data are copied from the FLASH to the Buffer by code, and then from Buffer to the IDAC using chained DMA. The IDAC is configured as a Source. The IDAC current is converted into voltage using 3.3k load resistor buffered by the Opamp in the follower mode, producing 0-1V signal at full scale.. For sound generation, the output is directly connected to the headphones with combined impedance of 64oHm (32+32).
Figure 2. Project annotation using the PSoC Annotation Library v1.0 and KIT-044. The Opamp output is directly loaded on the headphones with combined impedance of about 64oHm (32+32).
Figure 3. Output waveform on startup. The test data is Sawtooth, 256 points per period, played in the loop continuously.
Figure 4. Sawtooth waveform output when configured for a SINGLE_SHOT. The number of data points is 256, played once. After the end of data, the output can be set to some pre-defined value (here is 127).
Show Less
Id like to share this project, made a custom component, at the moment it is only enabled for PSoC4 but it can surely work with any other with minor changes( on PSoC 6).
the Communincation to the WS2812
no hardware blocks used
Github Repo:
Show LessThe evaluation board, CYBT-343026-EVAL, is not recognized even when inserted into a computer. There seems to be no driver software.
The board contains a USB Serial dual channel bridge controller (CY7C65215-32LTXI).
If you know how to install and enable the driver, please let me know.
Show LessOverview
Simple example to demonstrate a Master SPI configuration where the data movement is done with DMA channels (One for Master Transmit and the other Master Receive).
This project is using a standard ADS configuration and iLLD's. However the configuration of the QSP1, DMA channels 3 and 4 along with the ports are implemented in code as bare metal.
Description
In this code example, QSPI1 is configured as a master SPI. DMA channel 3 is used to transmit the data packet whereas DMA channel 4 is used to receive the data packet (SPI is use in full duplex mode. In this example the MTSR pin it externally connected to the MRST pin as there is not a real SPI slave device). The code directly accesses the registers for the QSPI and DMA. It doesn't use the iLLD's for these peripherals.
Clocks
* The system clock (PLL) is configured to run at 300MHz.
* The system peripheral bus is configured to run at 100MHz.
* The QSPI clock is fSOURCE2 configured to run at 200MHz.
Peripherals
* QSPI1
* DMA
Details to the Demo
The QSPI is operated in "Short Data Continuous Mode" When using this mode the transfer requires that you write two BACON entries. The first write is to begin the data exchange and ensure the LAST=0 at the start of the data transfer (it can also be used to remove any delay between the data on the bus). The other BACON write is used to close the data transfer before the last data value is written (i.e. LAST=1). In this example the DMA transmit interrupt is used to to write the last BACON and data value to complete the data exchange. Therefore the DMA transfer count for the TX is always one less than the receive DMA transfer count.
The SPI data exchange is initialized by writing the BACON word to the BACONENTRY register. This will cause the Tx DMA to send its data until the transmit count is zero. The receive DMA is also triggered by data being received from the QSPI. When both DMA counts go to zero interrupts are raised for the CPU.
The demo assumes you have data buffers of "8-bits" in size that are aligned on word boundaries. Where you have the choice to transfer the data using the DMA with either 8-bit, 16-bit or 32-bit width transfers. The QSPI and DMA will handle the choice from the below define "QSPI_DL" define. Additionally the QSPI will handle the Endianess of the bytes in both directions.
#define DMA_CH_SIZE_INT8 0
#define DMA_CH_SIZE_INT16 1
#define DMA_CH_SIZE_INT32 2
/*change this for the size of the DMA transfer, the endianess is handled by the QSPI */
#define QSPI_DL DMA_CH_SIZE_INT8
To RUN
When connected to a debugger you can set the variable "test=1" to kick off the SPI data exchange.
Scope plots
Example of one data exchange on the Master QSPI
* (channel 1, white) is P11.6 QSPI1 Master Clock Output
* (channel 2, tan) is P11.9 QSPI1 Master Transmit Output
* (channel 3, red) is P11.3 QSPI1 Master Receive Input B
* (channel 4, brown) is P10.5 QSPI1 Slave Select Output 9 (ECON1)
#define QSPI_DL DMA_CH_SIZE_INT8
#define QSPI_DL DMA_CH_SIZE_INT32
Hi,Community,
I created a project to start CAPSENSE Tuner with UART for PSoC4000S.
The CAPSENSE project borrows from the proximity sensing project(CE225691).
To use UART, only a few changes to the component and main.c are required.
STEP1: You need to change the SCB component from EZI2C to UART.
STEP2: You can either comment out or delete the code related to EZI2C in the original project.
This discussion will help you understand how to write a UART.
https://community.infineon.com/t5/PSoC-4/UART-packet-for-CapSense-Tuner/td-p/196830
To activate the CAPSENSE tuner via UART, please use MiniProg4. MiniProg3 is not suitable for its UART. Please refer to the caution note on page 10 of this document.
Once you have made the necessary changes to your project for UART, all you need to do is build it and then launch the CAPSENSE Tuner.
Best Regards,
Chihiro Tatebayashi / NEXTY
Hi,
Is there way to update the "Firmware Revision String" field in the GATT Device Information service at runtime? I can set the value using bt-configurator, but the actual firmware revision is set as part of our build pipeline so manually editing the value is not an option.
There's the `Cy_BLE_GATTS_WriteAttributeValueLocal()` function that looks promising, but I can seem to find the right attribute handle to use.
Show LessHi,
Recently I had a chance to write a sample program of multiple channel proximity sensor
https://community.infineon.com/t5/PSoC-4/About-proximity-sensor-detection-function/td-p/613161
There were a couple of things I wanted to touch up, as I tried to make the sample simple and easy, the code was somewhat clumsy and it did not support CapSense Tuner.
CapSense_ScanAllWidgets() ;
for(;;)
{
if (CapSense_NOT_BUSY == CapSense_IsBusy()) {
CapSense_ProcessAllWidgets() ;
prox[0] = CapSense_IsProximitySensorActive(
CapSense_PROXIMITY0_WDGT_ID, CapSense_PROXIMITY0_SNS0_ID) ;
prox[1] = CapSense_IsProximitySensorActive(
CapSense_PROXIMITY0_WDGT_ID, CapSense_PROXIMITY0_SNS1_ID) ;
prox[2] = CapSense_IsProximitySensorActive(
CapSense_PROXIMITY0_WDGT_ID, CapSense_PROXIMITY0_SNS2_ID) ;
prox[3] = CapSense_IsProximitySensorActive(
CapSense_PROXIMITY0_WDGT_ID, CapSense_PROXIMITY0_SNS3_ID) ;
if ((prox[0] != prev[0])
|| (prox[1] != prev[1])
|| (prox[2] != prev[2])
|| (prox[3] != prev[3])) {
snprintf(str, STR_LEN, "PROXY: 0:%d, 1:%d, 2:%d, 3:%d\n\r",
prox[0], prox[1], prox[2], prox[3]) ;
print(str) ;
}
prev[0] = prox[0] ;
prev[1] = prox[1] ;
prev[2] = prox[2] ;
prev[3] = prox[3] ;
CapSense_ScanAllWidgets() ;
}
}
So I rewrite the program something like below and added support of CapSense Tuner
CapSense_ScanAllWidgets() ;
for(;;) {
if (CapSense_NOT_BUSY == CapSense_IsBusy()) {
CapSense_ProcessAllWidgets() ;
#if USE_TUNER
CapSense_RunTuner() ;
#endif
if (update_prox()) {
#if !USE_TUNER
print_prox() ;
#endif
}
save_prox() ;
CapSense_ScanAllWidgets() ;
}
}
}
Usage
(1) When using with a serial terminal such as Tera Term
In the beggining of the main.c, please define USE_TUNER as 0
After building and loading the program to the board or start debugger,
Tera Term output was something like
(2) When using with CapSense Tuner
Note: Please close Tera Term connection to use CapSense Tuner
This time, please define USE_TUNER as 1
After Clean and Rebuild the program, load the program to the board
Then from the schematic page, select "CapSense" component with right button click and select "Launch Tuner"
Then CapSense Tuner window shows up
For the first time connection, select Menu: Tools > Tuner Communication Setup...
or select the "Tuner Communication Setup" icon located at the left side of the "connect" icon.
Then Tuner Communication Setup window shows up,
choose "I2C" port, Sub-address "2-Bytes"
Then select "Connect" icon
When connected to the CapSense Tuner the "Connect" button turns to "Disconnect" button
and at the bottom of the Senser Tuner, Bridge status: turns to "Connected"
Then select "Start" icon
Now both the program and CapSense Tuner should be running,
and according to the location of the hand(s) the values of each electrodes are shown
And if we switch the tab to Graph View signals are shown in a oscilloscope like style
Now some more details...
Schematic
CapSense Config
EzI2C Config
Note: Sub-address size was changed from 8 to 16
UART Config
Pins
main.c
#include "project.h"
#include "stdio.h"
#define USE_TUNER 0
#if !USE_TUNER
#define STR_LEN 64
char str[STR_LEN + 1] ;
void print(char *str) ;
void cls(void) ;
void splash(char *title) ;
void print_prox(void) ;
#endif
#define NUM_PROXY 4
int prox[NUM_PROXY] = { 0 } ;
int prev[NUM_PROXY] = { 0 } ;
int prox_wdgt_id[NUM_PROXY] = {
CapSense_PROXIMITY0_WDGT_ID,
CapSense_PROXIMITY0_WDGT_ID,
CapSense_PROXIMITY0_WDGT_ID,
CapSense_PROXIMITY0_WDGT_ID
} ;
int prox_sns_id[NUM_PROXY] = {
CapSense_PROXIMITY0_SNS0_ID,
CapSense_PROXIMITY0_SNS1_ID,
CapSense_PROXIMITY0_SNS2_ID,
CapSense_PROXIMITY0_SNS3_ID
} ;
int update_prox(void)
{
int result = 0 ;
int i ;
for (i = 0 ; i < NUM_PROXY ; i++) {
prox[i] = CapSense_IsProximitySensorActive(prox_wdgt_id[i], prox_sns_id[i]) ;
if (prox[i] != prev[i]) {
result = 1 ;
}
}
return(result) ;
}
void save_prox(void)
{
int i ;
for (i = 0 ; i < NUM_PROXY ; i++) {
prev[i] = prox[i] ;
}
}
int main(void)
{
CyGlobalIntEnable; /* Enable global interrupts. */
#if USE_TUNER
EZI2C_Start() ;
EZI2C_EzI2CSetBuffer1(
sizeof(CapSense_dsRam),
sizeof(CapSense_dsRam),
(uint8_t *)&(CapSense_dsRam)) ;
#else
UART_Start() ;
splash("Multi Proxy Test") ;
#endif
CapSense_Start() ;
CapSense_ScanAllWidgets() ;
for(;;) {
if (CapSense_NOT_BUSY == CapSense_IsBusy()) {
CapSense_ProcessAllWidgets() ;
#if USE_TUNER
CapSense_RunTuner() ;
#endif
if (update_prox()) {
#if !USE_TUNER
print_prox() ;
#endif
}
save_prox() ;
CapSense_ScanAllWidgets() ;
}
}
}
#if !USE_TUNER
void print_prox(void)
{
snprintf(str, STR_LEN, "PROXY: 0:%d, 1:%d, 2:%d, 3:%d\n\r",
prox[0], prox[1], prox[2], prox[3]) ;
print(str) ;
}
void print(char *str)
{
UART_UartPutString(str) ;
}
void cls(void)
{
print("\033c") ; /* reset */
CyDelay(20) ;
print("\033[2J") ; /* clear screen */
CyDelay(20) ;
}
void splash(char *title)
{
cls() ;
print(title) ;
snprintf(str, STR_LEN, "(%s %s)\n", __DATE__, __TIME__) ;
print(str) ;
}
#endif
That's the whole enchilada.
moto
Show Less
This code example can be used for interfacing of XENSIVTM Photoacoustic Spectroscopy (PAS) CO2 sensor with PSoC6 via I2C using available PSoC6 library. The document then explains the extension of the implementation to a CO2 traffic light.
Introduction
The document describes the procedure to interface XENSIV™ PAS CO2 sensor with PSoC6 evaluation board. The basic implementation covers the interfacing the sensor with PSoC6 and the CO2 levels measured is printed in the serial terminal. In this article based on the measured CO2 levels, three LED’s of different colors (green, orange/yellow and red) are individually turned on.
Hardware
The hardware required for the implementation are
- PSoC™ 6 Wi-Fi Bluetooth® pioneer kit
- XENSIV™ PAS CO2 mini-evaluation board or XENSIVTM PAS CO2 Shield2Go board
Figure 1. (a) XENSIV™ PAS CO2 Mini Evaluation Board (b) XENSIV™ PAS CO2 Shield2Go board
The setup using PAS CO2 mini evaluation board can be understood from the figure shown below.
Figure 2. Wiring connection for interfacing XENSIVTM PAS CO2 mini-evaluation board with PSoC™ 6 Wi-Fi Bluetooth® pioneer kit via I2C
The 12 V required for the sensor operation needs to be supplied externally. Please also keep the ground common in all the connections to ensure proper functionality.
PAS CO2 Shield2Go board can be used instead of the mini-evaluation board. The Shield2Go board can be interfaced with the PSoC™ 6 Wi-Fi Bluetooth® pioneer kit as shown in the figure below. Here the advantage is that there is no need for providing 12 V externally.
Figure 3. Wiring connection for interfacing XENSIVTM PAS CO2 Shield2Go board with PSoC™ 6 Wi-Fi Bluetooth® pioneer kit, via I2C
Once the hardware setup is ready, using any of the above options, please proceed to the software setup mentioned in the next section.
Software Setup
Steps required for the software implementation are listed below
Step 1: Please follow the steps from https://github.com/Infineon/sensor-xensiv-pasco2 to have the initial software setup in Modus Toolbox
Step 2: Include the following code for defining the GPIO pins for controlling red, yellow/orange and green LEDs. The calculated CO2 ppm values needs to be compared and used to determine the states of LED’s. For that purpose, a comparator loop can be added as shown below.
#include "cyhal.h"
#include "cybsp.h"
#include "cy_retarget_io.h"
#include "xensiv_pasco2_mtb.h"
/*******************************************************************************
* Macros
*******************************************************************************/
#define PIN_XENSIV_PASCO2_I2C_SDA CYBSP_I2C_SDA
#define PIN_XENSIV_PASCO2_I2C_SCL CYBSP_I2C_SCL
#if defined(USE_CYSBSYSDEV_KIT_01_WINGBOARD)
/* Output pin for sensor PSEL line */
#define PIN_XENSIV_PASCO2_PSEL P5_3
/* Output pin for PAS CO2 Wing Board power switch */
#define PIN_XENSIV_PASCO2_POWER_SWITCH P10_5
#endif
#define I2C_MASTER_FREQUENCY (100000U)
/* Wait time for sensor ready (milliseconds) */
#define WAIT_SENSOR_RDY_MS (2000)
/* The CO2 concentration value acquired by the sensor depends on the external atmospheric pressure.
To compensate for this effect, pressure values can be acquired from a pressure sensor such as an
Infineon XENSIV™ DPS3xx. (https://github.com/Infineon/sensor-xensiv-dps3xx) */
#define DEFAULT_PRESSURE_REF_HPA (0x3F7) /* Default atmospheric pressure to compensate for (hPa) */
/*Defining GPIO pins for LEDs*/
#define PIN_R P9_1
#define PIN_Y P9_4
#define PIN_G P9_7
/***********************************/
/*******************************************************************************
* Global Variables
*******************************************************************************/
static cyhal_i2c_t cyhal_i2c;
static xensiv_pasco2_t xensiv_pasco2;
int main(void)
{
/*Initializing GPIO pins for LEDs*/
cyhal_gpio_init(PIN_R, CYHAL_GPIO_DIR_OUTPUT,CYHAL_GPIO_DRIVE_STRONG, false);
cyhal_gpio_init(PIN_Y, CYHAL_GPIO_DIR_OUTPUT,CYHAL_GPIO_DRIVE_STRONG, false);
cyhal_gpio_init(PIN_G, CYHAL_GPIO_DIR_OUTPUT,CYHAL_GPIO_DRIVE_STRONG, false);
cy_rslt_t result = CY_RSLT_SUCCESS;
/* Initialize the device and board peripherals */
result = cybsp_init();
CY_ASSERT(result == CY_RSLT_SUCCESS);
__enable_irq();
/* Initialize retarget-io to use the debug UART port. */
result = cy_retarget_io_init(CYBSP_DEBUG_UART_TX, CYBSP_DEBUG_UART_RX, CY_RETARGET_IO_BAUDRATE);
CY_ASSERT(result == CY_RSLT_SUCCESS);
printf("XENSIV PAS CO2 Example\r\n");
/* Initialize I2C */
cyhal_i2c_cfg_t i2c_master_config = {CYHAL_I2C_MODE_MASTER,
0,
I2C_MASTER_FREQUENCY};
result = cyhal_i2c_init(&cyhal_i2c, PIN_XENSIV_PASCO2_I2C_SDA, PIN_XENSIV_PASCO2_I2C_SCL, NULL);
CY_ASSERT(result == CY_RSLT_SUCCESS);
result = cyhal_i2c_configure(&cyhal_i2c, &i2c_master_config);
CY_ASSERT(result == CY_RSLT_SUCCESS);
#if defined(USE_CYSBSYSDEV_KIT_01_WINGBOARD)
/* Initialize and enable PAS CO2 Wing Board I2C channel communication*/
result = cyhal_gpio_init(PIN_XENSIV_PASCO2_PSEL, CYHAL_GPIO_DIR_OUTPUT, CYHAL_GPIO_DRIVE_STRONG, false);
CY_ASSERT(result == CY_RSLT_SUCCESS);
/* Initialize and enable PAS CO2 Wing Board power switch */
result = cyhal_gpio_init(PIN_XENSIV_PASCO2_POWER_SWITCH, CYHAL_GPIO_DIR_OUTPUT, CYHAL_GPIO_DRIVE_STRONG, true);
CY_ASSERT(result == CY_RSLT_SUCCESS);
#endif
cyhal_system_delay_ms(WAIT_SENSOR_RDY_MS);
/* Initialize PAS CO2 sensor with default parameter values */
result = xensiv_pasco2_mtb_init_i2c(&xensiv_pasco2, &cyhal_i2c);
if (result != CY_RSLT_SUCCESS)
{
printf("PAS CO2 device initialization error");
CY_ASSERT(0);
}
#if defined(USE_CYSBSYSDEV_KIT_01_WINGBOARD)
/* Configure PAS CO2 Wing board interrupt to enable 12V boost converter in wingboard */
xensiv_pasco2_interrupt_config_t int_config =
{
.b.int_func = XENSIV_PASCO2_INTERRUPT_FUNCTION_NONE,
.b.int_typ = (uint32_t)XENSIV_PASCO2_INTERRUPT_TYPE_LOW_ACTIVE
};
result = xensiv_pasco2_set_interrupt_config(&xensiv_pasco2, int_config);
if (result != CY_RSLT_SUCCESS)
{
printf("PAS CO2 interrupt configuration error");
CY_ASSERT(0);
}
#endif
uint16_t ppm;
/*Defining CO2 ppm levels for safe and warning*/
uint16_t co2ppmsafe = 800;
uint16_t co2ppmwarn = 1100;
for (;;)
{
result = xensiv_pasco2_mtb_read(&xensiv_pasco2, DEFAULT_PRESSURE_REF_HPA, &ppm);
if (result == CY_RSLT_SUCCESS)
{
printf("CO2 %d ppm.\r\n", ppm);
if(ppm<=co2ppmsafe)
{
cyhal_gpio_write(PIN_G,true);
cyhal_gpio_write(PIN_Y,0);
cyhal_gpio_write(PIN_R,0);
}
else if(ppm>co2ppmsafe && ppm<=co2ppmwarn)
{
cyhal_gpio_write(PIN_G,0);
cyhal_gpio_write(PIN_Y,true);
cyhal_gpio_write(PIN_R,0);
}
else if (ppm>co2ppmwarn)
{
cyhal_gpio_write(PIN_G,0);
cyhal_gpio_write(PIN_Y,0);
cyhal_gpio_write(PIN_R,true);
}
}
cyhal_system_delay_ms(10);
}
}
Step 3: The output can be seen in the terminal as shown in Figure 4.
Figure 4. CO2 ppm levels being printed in the serial terminal
The LED’s will be turned on/off based on the CO2 ppm values measured as seen in Figure 5.
Figure 5. LEDs showing the status of CO2 ppm levels, (a) safe state, (b) warning state and (c) danger state
Green LED can show that the environment is safe. Orange/Yellow LED can show a warning state and can be used to initiate some preventive measures. The preventive measures can be as simple as controlling the air conditioning unit or opening the windows. The Red LED can indicate a worst working environment and should be followed by strict actions like vacating the room. A better understanding of effects of CO2 levels on human comfort levels can be understood from Figure 6.
Figure 6. Human comfort levels based on CO2 ppm levels
Working condition is very comfortable for CO2 levels below 800 ppm. Beyond this level the conditions start deteriorating and working condition becomes difficult as CO2 levels reaches 1200 ppm. It is not recommended to continue working with CO2 levels more than 1200 ppm and is considered danger. Continuing working in these conditions can cause headache and sleepiness initially. Further higher levels of CO2 is harmful for human life and is extremely dangerous.
References
Show LessA new version of the component (v.1.0) is provided below
Provided below is custom component (SerialPlot v0.0) for interfacing with real-time plotting software SerialPlot.
Hackaday.io: SerialPlot - Realtime Plotting Software
The component implements interface to the real-time charting software SerialPlot. Using this component, PSoC data can be easily visualized on personal computer (Linux, Mac & Windows). Component doesn’t consume hardware resources, performing all operations by CPU, which is useful for systems with little resources, such as PSoC4. Multiple instances of the component can run simultaneously in the project.
Component features:
Data types: int8, int16, int32, uint8, uint16, uint32, float
Up to 8 channel output
The component was tested using CY8KIT-059 PSoC5 prototyping kit and CY8KIT-042 PSoC4 Pioneer Kit. Demo projects are provided.
Attached archive contains component library, component datasheet and demo projects for PSoC5 and PSoC4. Please read installation instructions in the readme.txt.
The component provided as-is, no liabilities. It is free to use and modify.
/odissey1
P.S. Demo projects use optional annotation components (which are also provided here in Support_libs.zip):
PSoC Annotation Library: PSoC Annotation Library v1.0
KIT-042 annotation stub: KIT-042: annotation component for CY8CKIT-042 Pioneer Kit
Download SerialPlot: Hackaday.io: SerialPlot - Realtime Plotting Software
Figure 1. SerialPlot demo project schematic.
Figure 2. Project data output to SerialPlot graphic software.
Show Less