Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Code Examples Forum Discussions

shsh_4753781
Code Examples
Hello, I am trying to use two I2S instances to design a project for collecting data using im69d130 microphone shield2go from Infineon. As per the data... Show More
Suma
Code Examples
Hello.... Starting with Cypress controller, what development kit or code examples helps me to develop small test application to verify the proper work... Show More
Len_CONSULTRON
Code Examples
I've attached a project that has DMA-driven function equivalents for: memset() => dmemset() memcpy() => dmemcpy() memmove() => dmemmove() It uses a ... Show More
MotooTanaka
Code Examples
In the discussion below,   下記のスレッドで   https://community.cypress.com/t5/PSoC-General/I-could-not-find-TCPWM-on-the-Component-Catalog-PSoc-4-4/m-p/278399#M222... Show More
Kenshow
Code Examples
Hello, I was approached by someone who required to use the PC's BLE instead of Uart serial to output PSoC logs and data. And since there was no sample... Show More
YoIs_1298666
Code Examples
Hello, I have prepared a sample project for interrupt processing from GPIO pins of the same port group. This is based on "7.8 Pin Interrupt" in AN8643... Show More
Michcfr
Code Examples
Hello, is there any sample code (Arduino?) for the CY8C95xxx IO expander? Thank you Michel     Show More
BRFL_4822626
Code Examples
Hello:I am trying to add a custom service to the example code in CE217643 i.e. the BLE Temperature Measurementwith PSoC 6 MCU with BLE Connectivity, H... Show More
JoJo_4453281
Code Examples
Using the CY8CKIT-149 PSoC® 4100S Plus Prototyping Kit, what view the touchpad serial data in a terminal emulator? Reading serial data is a very impor... Show More
BhSa_4078721
Code Examples

Hi,

Can i get any sample code for water tolerance. How guard sensor is handle in code???