Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Code Examples Forum Discussions

YoIs_1298666
Code Examples
Hello, This sample code implements SmartIO's Count Up Wrap function using a TCPWM line clock. TCPWM line is connected to the data4 of SmartIO. GND i... Show More
YoIs_1298666
Code Examples
Hello, This sample code implements SmartIO's Match DATA1 function using a GPIO input clock.TCPWM_CLK is connected to the gpio4 of SmartIO. TCPWM_SHIF... Show More
YoIs_1298666
Code Examples
Hello, This is a sample code of SmartIO that wakes up from DeepSleep without using WDT. Since the SmartIO counter is 8 bits, it can only count up to 6... Show More
MotooTanaka
Code Examples
Hi, こんにちは、   I found the following discussion 下記のようなスレッドを見つけました https://community.infineon.com/t5/PSoC-5-3-1/a-way-to-use-millies-from-arduino-in-Psoc/td-p/328317... Show More
RodolfoGL
Code Examples
I saw a few times requests to create a bi-directional level translator. It is pretty straight forward to do an unidirectional level translator with PS... Show More
MotooTanaka
Code Examples
Hi, In the following discussion,  https://community.infineon.com/t5/PSoC-5-3-1/PSOC5-LP-with-4x4-Keypad-and-16x2-LCD-Menu-System-Example/m-p/327255#M46127... Show More
MotooTanaka
Code Examples
Hi, In a discussion below, the problem seemed to be complicate, so I ordered the similar PCF 8563 RTC Module to test with, https://community.infineon.com/t5/PSoC-5-3-1/PSOC-5LP-interfacing-with-WaveShare-PCF-8563-RTC-module-not/m-p/324987#M46011... Show More
Len_CONSULTRON
Code Examples
  UPDATE: 11.07.2021 in BLUE. I've created a relatively simple sinewave generator for audio testing applications.  It uses a CY8CKIT-059, CY8CKIT-030,... Show More
MotooTanaka
Code Examples
Hi, in my previous sample discussion below, I received a question/request for CY8CPROTO-063-BLE. https://community.cypress.com/t5/Code-Examples/CharLCD-Sample-for-PSoC-6-CY8CKIT-062-BLE/m-p/268325#M1017... Show More
SaGa_4641021
Code Examples
Hi I am using a code example (CE218964 - PSoC 6 MCU RTC Daily Alarm). the printf() functions does not print to serial port. I had the same issue with ... Show More