- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
A new version of the component (v.1.0) is provided below
Provided below is custom component (SerialPlot v0.0) for interfacing with real-time plotting software SerialPlot.
Hackaday.io: SerialPlot - Realtime Plotting Software
The component implements interface to the real-time charting software SerialPlot. Using this component, PSoC data can be easily visualized on personal computer (Linux, Mac & Windows). Component doesn’t consume hardware resources, performing all operations by CPU, which is useful for systems with little resources, such as PSoC4. Multiple instances of the component can run simultaneously in the project.
Component features:
Data types: int8, int16, int32, uint8, uint16, uint32, float
Up to 8 channel output
The component was tested using CY8KIT-059 PSoC5 prototyping kit and CY8KIT-042 PSoC4 Pioneer Kit. Demo projects are provided.
Attached archive contains component library, component datasheet and demo projects for PSoC5 and PSoC4. Please read installation instructions in the readme.txt.
The component provided as-is, no liabilities. It is free to use and modify.
/odissey1
P.S. Demo projects use optional annotation components (which are also provided here in Support_libs.zip):
PSoC Annotation Library: PSoC Annotation Library v1.0
KIT-042 annotation stub: KIT-042: annotation component for CY8CKIT-042 Pioneer Kit
Download SerialPlot: Hackaday.io: SerialPlot - Realtime Plotting Software
Figure 1. SerialPlot demo project schematic.
Figure 2. Project data output to SerialPlot graphic software.
- Labels:
-
ispn:39611:1:0
-
l1:314:1:0
-
PSoC345LP
- Tags:
- annotation library
- chart
- charting
- community component
- cypress
- data output
- kit-042
- kit-059
- library
- odissey1
- plot
- plotting
- psoc
- serial
- serial plot
- serialplot
- uart