- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Provided below is the Annotation Library - a set of external components intended for documenting PSoC schematics. It consists of more than 40 components (Resistor, Capacitor, Opamp, etc.) designed for visualizing external connections to the PSoC prototyping kits.
The Library complements Creator stock off-chip annotation components. It doesn’t consume system resources, nor affects run-time performance of the project. The Library was tested OK with Creator 4.0 and 4.2. It is not specific to PSoC4, PSoC5 or PSoC6 and can be used in conjunction with KIT-042, KIT-044 and KIT-059 annotation components:
Annotation component for CY8CKIT-042 Pioneer Kit
Annotation component for CY8CKIT-044 PSoC4M Pioneer Kit
KIT-059: annotation component for CY8CKIT-059 PSoC5LP Prototyping Kit
The Library includes by default the KIT-059 annotation stub for CY8CIT-059 PSoC5LP Prototyping Kit.
Attached archive contains the Annotation Library, Datasheet, Demo project and readme file. Upon installation the Library will show up in the Component Catalog Panel, path:
/Community/Off-Chip/Annotation Library/
The Library provided as-is, no liabilities. It is free to use, modify and distribute.
regards,
odissey1
Figure 1. List of components included in the Library (v1.0)
Figures 2. Example of schematic created using Annotation Library and KIT-059 stub.
Figure 3. Example of sensor schematic created using Annotation Library and KIT-059 stub.
Figure 4. Example of sensor schematic created using Annotation Library and KIT-044 stub.
- Labels:
-
PSoC 345 LP
-
PSoC 6
- Tags:
- annotation
- annotation component
- annotation library
- community component
- cypress
- kit-042
- kit-044
- kit-059
- library
- odissey1
- off-chip component
- pioneer board
- pioneer kit
- prototyping kit