Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Code Examples

odissey1
Level 9
First comment on KBA 1000 replies posted 750 replies posted
Level 9

Hi,

Provided below is the Annotation Library - a set of external components intended for documenting PSoC schematics. It consists of more than 40 components (Resistor, Capacitor, Opamp, etc.) designed for visualizing external connections to the PSoC prototyping kits.

The Library complements Creator stock off-chip annotation components. It doesn’t consume system resources, nor affects run-time performance of the project. The Library  was tested OK with Creator 4.0 and 4.2. It is not specific to PSoC4, PSoC5 or PSoC6 and can be used in conjunction with KIT-042, KIT-044 and KIT-059 annotation components:

Annotation component for CY8CKIT-042 Pioneer Kit

Annotation component for CY8CKIT-044 PSoC4M Pioneer Kit

KIT-059: annotation component for CY8CKIT-059 PSoC5LP Prototyping Kit

The Library includes by default the KIT-059 annotation stub for CY8CIT-059 PSoC5LP Prototyping Kit.

Attached archive contains the Annotation Library, Datasheet, Demo project and readme file. Upon installation the Library will show up in the Component Catalog Panel, path:

/Community/Off-Chip/Annotation Library/

The Library provided as-is, no liabilities. It is free to use, modify and distribute.

regards,

odissey1

Figure 1. List of components included in the Library (v1.0)

AnnLib_sm1_F2.png

Figures 2. Example of schematic created using Annotation Library and KIT-059 stub.

PID_ex_01_E.png

Figure 3. Example of sensor schematic created using Annotation Library and KIT-059 stub.

Demo_ex1_E.png

Figure 4. Example of sensor schematic created using Annotation Library and KIT-044 stub.

KIT-044_GLCD_A.png

1 Reply
Praveen
Community Manager
Community Manager 250 sign-ins 100 sign-ins 50 replies posted
Community Manager

Thanks for sharing this odissey1.

Very useful for the community!!

Nice detailed documentation !!

Cheers

Praveen

Cheers
Praveen
0 Likes