Here is the C# source code to a terminal program for a Windows PC.
Minimum System Requirements:
This code started as a simple PSoC UART (remote) to PC terminal application to replace Teraterm, Termite, RealTerm, etc.
I did this to eventually enhance the UART comm capabilities to include features such as
This code has those features built in by using my packetizing protocol.
Disclaimer
You are allowed to use this source code “at-will” for commercial or non-commercial purposes. I DO NOT state or imply any warranty for the use of this code in-whole or in-part.
I've attached an archive of the source code and a .pdf that describes the use and the packetizing protocol.
Len
Message was edited by: Len Removed bin and obj directories. Makes for a smaller .zip. Will be rebuilt when compiled.
Thank you Len for sharing this project!
Thank you so much for sharing this source code... This is great!!!
Regards
Normanj