New LED Matrix Driver Component (Max 24 Segments and Max 16 Commons)

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
Len_CONSULTRON
Level 9
Level 9
Beta tester 500 solutions authored 1000 replies posted

To all,

Here is a new LED matrix driver component.   It is highly based on the Cypress/Infineon component of the same type except it extends the number of maximum Commons from 8 to 16.

It uses the Cypress API interface and should be directly compatible to the Cypress component with the following exception:

  • The Brightness feature works globally on the entire display whereas the Cypress component allowed for individual Brightness based on the digit position.

Target PSoCs:

  • PSoC5 (Tested)
  • PSoC4 (Compiled without errors but not tested)

If you find issues with this component, please send me private messages.  I will see what I can do to apply a fix.

Len
"Engineering is an Art. The Art of Compromise."
1 Reply
Rakshith
Moderator
Moderator
Moderator
250 likes received 1000 replies posted 750 replies posted

Hi Len, 

Thanks a lot for sharing this with the community! 🙂

Best Regards, 
Rakshith 

Thanks and Regards,
Rakshith M B
0 Likes