- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi all,
The electronic dice I posted last time was very popular. So, I add a piezoelectric buzzer to generate sound with PWM. Please refer to the link for details regarding the electronic dice and the piezoelectric buzzer of PWM.
The environment used is as follows:
・PSoC Creator 4.2
・CY8CKIT-062-BLE
The counter of the dice used the timer last time, but I changed it to PWM (PWM_1) because I want to control the length of the sound with Low/High signales. It is PWM_2 that produces the beep sound. PWM_2 used Start and Stop (Kill) inputs to control the blinking of the LED and the duration of the sound. The circuit is as follows:
The period of PWM_1 is set to the same period as the previous timer setting (Period0 = 399: 25Hz). Compare0 is set to 200 as the length of beep.
PWM_2 determines the frequency of the beep. This time, it is set to 2KHz (input clock is 1MHz, Period=499). Compare0 is 200 counts and is fixedly used in the program. The settings are as follows:
In the Advance tab, set Start Input to Rising Edge and Kill Input to Falling Edge to enable Start and Stop (Kill) inputs.
The buzzer pin is set to P12 [0] and the other pins are set as follows:
The program contains the control of PWM_1and 2.
#include "project.h"
uint32_t sw=0; //sw is off (Stop rolling dicce)
int main(void)
{
__enable_irq(); /* Enable global interrupts. */
/* Place your initialization/startup code here (e.g. MyInst_Start()) */
Clock_Enable() ;
CapSense_Start();
CapSense_ScanAllWidgets(); // Start Initial Scan
for(;;)
{
if(!CapSense_IsBusy())
{
CapSense_ProcessAllWidgets();
if(sw==0){ // If sw is on, check start botton0.
if(CapSense_IsWidgetActive(CapSense_BUTTON0_WDGT_ID)) // Check button 0 state
{
/* Start rolling dice*/
PWM_1_SetCounter(0);
PWM_1_SetPeriod0(399);
//PWM_1_SetCompare0(200);
PWM_1_Start(); // Start rolling dice
PWM_2_Start();
sw=1; // sw is on
}
}
if(sw==1){ // If sw is on, check stop botton0.
if(CapSense_IsWidgetActive(CapSense_BUTTON1_WDGT_ID)) // Check button 1 state
{
/* Roll dice slowly */
PWM_1_SetCounter(0);
PWM_1_SetPeriod0(1999);
//PWM_1_SetCompare0(200);
CyDelay(1500); // keep rolling slowly for 1.5sec
PWM_1_Disable();// Stop rolling dice
PWM_2_Disable();
sw=0; // sw is off
}
}
CapSense_UpdateAllBaselines();
CapSense_ScanAllWidgets(); // Start next scan
}
}
}
Thanks,
Kenshow
- Labels:
-
PSoC 6